• HMC1106

    Does the HMC1106 come in a chip package?  The datasheet implies it is only available as a die. 

  • HMC1106 mixer as upconverter

    Hello everybody,

    I am going to use HMC1106 in a design. I would like to know if it can be used as an upconverter.

    I have an input signal from 4 GHz to 20 GHz. I want to mix it with a local oscillator from 28 GHz to 44 GHz and take the output at 24 GHz…

  • Inquiry of HMC1106 specification

    Hello all,

    I could not find IF Return Loss Response data of HMC1106 in the datasheet.

    Could you please provide IF Retrun Loss Response data of HMC1106, such as the sample below ?

    Thanks in advance.

  • RE: I am building Footprints for our Library and am looking for DXF files.

    Please create separate posts requesting die dimensions for the following products:

    HMC8410CHIPS

    HMC-ALH476

    HMC1106

    BTW, each datasheet has figures with die dimensions and bond pad locations.