• HMC1097 - Phase error

    I am testing HMC1097 currently and my IQ input frequency of 35 Mhz, LO 467Mhz
    The results of RF_out have been obtained that the upper and lower boundary frequencies are:

    432Mhz (-19dbm), 501Mhz (-29dbm). According to Specifications, the 501Mhz component…

  • HMC1097 driven by quadrature hybrid

    I'd like to use an HMC1097 as an image-rejection upconverter to go from 70 MHz to 500 MHz. The 70 MHz signal comes from an existing single-ended source, not a DAC. Would I be able to transformer couple the I and Q inputs as shown below to convert from…

  • Bias Circuit on the HMC1097

    Does the bias circuit that the EN pin controls, produce the DC common-mode voltage for the differential baseband inputs (QP, QN, IP, and IN)? 

  • RE: HMC1097

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: HMC1097

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: HMC1097 IQ baseband bandwidth?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • HMC1097 EVAL

    Hello.

    I've gotten HMC1097 EVAL PCB file.

    They use substrate as Rogers 4350(0.01inch, 0.254mm) and 16mil signal line.

    Is it microstrip line or CPWG?

    When I calculate line impedance, there are 60ohm line...

    1,6,13,15 pins are N/C and these pins…

  • ad-fmcdaq2 and eval01-hmc1097 single-ended

    we want to use the ad-fmcdaq2 board to drive the hmc1097 eval board. however, the output of the ad-fmcdaq2 is single ended while the hmc1097 eval board input is differential. can we just 50ohm terminate the N channel of the hmc1097 BB_I/Q and connect…

  • Inquiry of AD9122 & HMC1097 design

    Hi all,

    My customer will use AD9122 & HMC1097 for 700MHz ~ 3000MHz freq band.

    Could you provide a design reference information about AD9122 & HMC1097 as below?

       http://www.analog.com/media/en/reference-design-documentation/reference-designs…

  • Frequency range of I/Q base band input port on HMC1097

    Hello, 

    My customer would like to know the frequency range for the I/Q input. They want to have quadrature modulation for the GHz  Lo input with 100MHz to 500MHz base band. However, no frequency range explanation for I/Q input in the data sheet. Please let…