• RE: HMC1087F10 missing specifications

    Hi vgoyal_hrd,

    1) Typical duty cycle is 100us for this part.

    2) I do not believe we have a CW AMR number for this part if that’s what you’re asking.

     

    Thanks,

    Dan

  • HMC1087F10 heat sink

    Do I need a heat sink for the HMC1087f10? If so is there a recommended vendor and part number?

  • HMC1087F10 evaluation board RF OUT port coupling?

    HMC1087-Die and HMC1087F10 has different coupling at RF out on their datasheet. Could you confirm that RF out is AC coupled at HMC1087F10 and at its evaluationboard?

  • HMC1087

    Hello,

    Do you have noise figure data for the HMC1087, or the HMC1087F10? Thanks.

    Best Regards.

  • RE: X-band Driver and PA

    Hi Sai,

    I suggest that you look at the following amplifiers from our catalog:

    Hittite Microwave - HMC487LP5, Linear & Power

    Hittite Microwave - HMC1087F10, GaN Power Amplifiers

    Regards,

    SMcBride

  • HMC1087-DIE and HMC1087F10_1GHZ~2GHz RF performance

    Dear team,

    I am reviewing the HMC1087-DIE and HMC1087F10 for the wide band HPA design.

    Can I get  the RF performance data at 1GHz~2GHz?

    - Gain

    - Psat

    -P1dB

    Thank you.

    Best regards,

    Josh

  • RE: Step model for HMC1086F10

    Hi Craig,

    The Gerber files, including complete stack-up info, are located here:

    http://www.analog.com/media/en/technical-documentation/evaluation-documentation/gerber-files/hmc1086f10-hmc1087f10-gerber.zip

    Do those suit your requirements, or are you…

  • RE: FMCOMMS1-4 custom Signal Path

    Hi Luis,

     

    On the receive side, I would recommend the ADL5523 which has a noise figure of around 1 dB. A better choice might be HMC667LP2E which is optimized for operation from 2.3 to 2.7 GHz and has a noise figure of 0.75 dB.

     

    On the transmit side…

  • RE: RF Amplifer for Keysight Genesys

    The attached list details all of the ADI RF Amplifier Sys-Parameter models that are available in the 2015.08 release of Keysight Genesys.  This library will be updated over time.

       

    PartNumber RealPartNumber Description