• RE: HMC1061 gerber files

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • HMC1061 and HMC661 thermal resistance

    Hi,

    Can you provide the junction-to-case thermal resistance (both top and bottom) of HMC661 and HMC1061?

    Thank you.

  • HMC1061LC5 Max Input Frequency

    Is it possible to operate HMC1061 at frequencies beyond 18 GHz.  Is it fundamentally not possible or will the device operate with degraded performance.

  • RE: HMC1061LC5

    1. Yes. The Absolute Max listed in the datasheet is per pin, applies to each pin.

    2. Strictly speaking, the sampling transfer function plot applies at the output of the HMC1061 device. However, we also show another plot right next to it on the same page…

  • EVAL01-HMC1061LC5 Power connector

    What is the PN of the 9-pin header used on the HMC1061 eval board?  And also, what is the pinout for the connector?  I can partially see the silkscreen labels from a picture of the eval board, but I wanted to get confirmation.

    Thanks

  • HMC661 operating temperature

    Hi,

    Can I confirm the operating temperature for HMC661 is 0 to 85 deg, and for HMC1061 is from -40 to 85deg?

    Thank you.

  • 3月重点推荐——民用雷达解决方案,是你的菜么?

    雷达广泛用于民用应用,从执法部门实施的汽车系统和速度监控到空中交通管制、天气和海上监控。雷达发射无线电波,然后通过其路径中的物体反射。雷达接收机处理这些反射波以确定物体的范围、角度或速度。例如,海上雷达可测量船舶方位和距离以防碰撞并进行船舶导航。在港口或海湾处,船舶交通服务雷达系统用于监控和调节繁忙水域中的船舶运动。配合飞机应答机系统一起使用的类似民用空中交通管制雷达确定相似特性,以确保飞机之间保持安全距离并协调飞行路径。

    主要挑战和系统设计考虑

    远程监控雷达,如空中交通管制、天气和海上雷达…

  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF