• HMC1055

    Friends,

    Intendto use HMC1055 for protection application with 2860 MHz.

    Please clarify RF1 (as OUT), and RF2 (as IN) are interchangeable?

    I intend to provide the RF2 port with internal termination, to which RF signal generator is connected.

    Kindly note…

  • HMC1055 SPST

    We are using HMC1055 SPST switch, the issue is that the switching signal on the Vctrl line leaks into RF path through the device - is there a way to get rid of switching signal leaking into RF lines from the Control line. Our switching frequency is less…

  • RE: HMC1055LP2CE

    Hello;

    Thank you for seeking to help me! I am confused over the two attachments with the "exact" same name.

    Is on for the HMC1055 when it is selected and the other for when it is not?

    Will the new/revised datasheet be available soon?

    Please…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • 总有一款适合您——最新《RF和微波IC选型指南》PDF免费下载ing

    天线到数字以及数字到天线……ADI凭借领先的射频技术能力、系统知识与工艺技术,提供直流到90 GHz以上、涵盖整个RF信号链最丰富多样的RF IC组合。

     

    面对上千款的RF IC产品,如何选出最适合自己应用的哪一款呢?ADIRF和微波IC》最新选型指南来帮您。(附件)

     

    最新版的《RF和微波IC》选型指南主要包括RF放大器、可变增益放大器、衰减器、RF混频器、I/Q调制器和解调器、集成式收发器……


  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF