• HMC1049LP5E OIP2

    I have an application where the HMC1049 amplifier is being used in a multi-octave wideband receiver front-end. The OIP2 is not mentioned in the spec sheet and I need to understand the second-order non-linearity properties. 

  • HMC1049LP5E dependancy  Idd from Gate Bias Voltage .

    Hi!

    How can I get diagram dependancy  Idd  (typical 70 mA) from Gate Bias Voltage, Vgg1 (-2V to +0.2V) ? Such dependancy is one and the same for all  HMC1049LP5E samples or can be individual for each HMC1049LP5E sample? 

    Thanks!

  • I want to use the HMC920LP5E Active Bias Controller with the HMC1049LP5E LNA.

    I want to use the HMC920LP5E Active Bias Controller with the HMC1049LP5E LNA.

    The data sheet for the HMC1049LP5E is not one of the amplifies listed in the HMC920LP5E's

    data sheet. The list also provides resistor values for the given amplifier.

  • HMC1049

    Hi, I am using HMC1049LP5E. The RF input is DC coupled. What is the  maximum DC bias  voltage can I apply to the FR input pin. Can I use ACG3, ACS2 pins to DC bias HMC1049?

  • hittite的放大器芯片HMC1049问题

    尊敬的工程师们,请教一下HMC1049的问题。

    HMC1049LP5E 芯片的RF输入输出引脚均是DC耦合,通常DC耦合是需要在输入输出端加上隔直电容的,但是其评估板却没有加隔直电容,直接将输入输出引脚引入到了SMA接口。

    所以问题来了,到底隔直电容是否必须呢。尤其是当使用HMC1049LP5E级联电路时,级间是否必须加隔直电容呢。

  • Request for data behind plots in datasheets

    I’d like to calculate the frequency dependent noise figure and OIP3 of a composite system I am simulating. Would it be possible to get the raw data behind the follow plots from the following datasheets?

    • HMC1049LP5E Rev. B
      • Figure 14. Noise Figure…
  • RE: RF Amplifer for Keysight Genesys

    The attached list details all of the ADI RF Amplifier Sys-Parameter models that are available in the 2015.08 release of Keysight Genesys.  This library will be updated over time.

       

    PartNumber RealPartNumber Description
  • 3月重点推荐——民用雷达解决方案,是你的菜么?

    雷达广泛用于民用应用,从执法部门实施的汽车系统和速度监控到空中交通管制、天气和海上监控。雷达发射无线电波,然后通过其路径中的物体反射。雷达接收机处理这些反射波以确定物体的范围、角度或速度。例如,海上雷达可测量船舶方位和距离以防碰撞并进行船舶导航。在港口或海湾处,船舶交通服务雷达系统用于监控和调节繁忙水域中的船舶运动。配合飞机应答机系统一起使用的类似民用空中交通管制雷达确定相似特性,以确保飞机之间保持安全距离并协调飞行路径。

    主要挑战和系统设计考虑

    远程监控雷达,如空中交通管制、天气和海上雷达…