• HMC1048A based on GaAs?

    Hello,

    It is not mentioned in the HMC1048A that the MMIC technology is based on GaAs.

    However, it is the case for the HMC1048 (obsolete), as indicated in the datasheet.

    Can you confirm/infirm that the HMC1048A is also still based on GaAs MMIC?

    Thank you…

  • RE: External 90º Hybrid for HMC525ALC4

    Hi,

    Using only one IF port without the hybrid would mean that you would have 3dB additional conversion loss. The hybrid is needed for image rejection. However you would lose the image rejection capability if using only one IF port.

    I think for your application…

  • RE: MC1048A Dynamic range

    Hi,

    The HMC1048A has not been released yet and won't be released till Q1 2018.

    I tested this with the HMC1048 mixer and the mixer downconverts for X Band RF signals at -100dBm. Even so, I do advise to use an RF LNA in your receiver before directly…

  • ADI针对电子测试和测量的RF和微波解决方案,优势在哪?

    RF和微波IC广泛用于电子测试和测量仪器,比如频谱分析仪、网络分析仪、信号发生器和通信测试仪。当无线通信在我们的生活中变得越来越普及,比如4G/5G和物联网,对于它们的测试基准的要求也在不断提高。在ADI针对电子测试和测量的RF和微波解决方案中,重点讨论ADI产品如何融入相关信号链。

    主要挑战和系统设计考虑


    宽动态范围

    最小化RF测试台的噪底(比如相位噪声)对于保持宽动态范围内的测试信号纯度很重要。但是,更多的数字信号处理任务将增加辐射噪声,因此获得干净的信号是个难题。

    宽带宽

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF