Hi Freddy,
s2p is already at ADI web page.
Package:
https://www.analog.com/en/products/hmc1040lp3ce.html
Die:
https://www.analog.com/en/products/hmc1040-die.html
Regards
Ivan S
Where can I find s-parameters for the following devices?
AD8340
HMC1040
ADAR2001
ADPA1122
HMC406
Hi all,
Our customer application is the parallel amps & mixer layout for Rx radar,
and severely space limited, so a simplified local decoupling scheme is preferred.
The data sheets for the HMC1040 & HMC 1093 shows that all three power supply pins…
Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.
How can I determine the die temperature of your device?
I wanted to Simulate the HMC392A in Microwave office. So i downloaded its S2P file from design resources and as i performed simulation its responses like return loss is better than the datasheet but its gain is decreased to max15.7 dB after simulation…
Hello,
Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing 220 mA @ 5volts, with no input signal or output load. Thanks.
Best Regards.
The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.
does the assumption that it will work if properly heatsunk although the…
Please provide S-parameters for HMC939A-DIE. Thanks.