Could you please provide the gerber files for the evaluation board EVAL01-HMC1030LP5E for layout guidance? Thanks.
Hi everyone,
I want to use HMC1030 to measure the power of baseband I and Q signal in order to calculate the power of the signal before demodulation. Does the HMC1030 can measure the power for baseband I/Q signal?
If there is other option, I really…
On behalf of Eamon Nash.
Unfortunately, this will not work. The ADL5920’s max input power is hardwired at +30 dBm. I think that there may be scope to increase this to +33 dBm but definitely not to 55 dB. I think that your only option is to use conventional…
It looks like the AD8364 does indeed have significant output voltage variation vs frequency. The attached plot shows how the output would vary vs frequency if each device was calibrated at a single frequency. For AD8364 (light blue), you can see that…
Dear Staff and fellows;
I need an envelope detector working at -55C. My frequency of operation is 60 +/-3 MHz. I was hoping to use ADL5910, but I was guided -by sales representative- as I can not use ADL5910 IC for envelope detection.
Then the choices…
Question: If I’m using a device such as AD8364 or HMC1030 to measure VSWR, how do I actually get from output voltage (or ADC code) to VSWR?
Answer: The short answer is that the return loss in dB is proportional to the differential voltage that…