• thermal resistance HMC1020

    Could anyoneone clarify and give me any advice?

    My customer would like to know thermal resistance of θja, θjc and θjb for HMC1020.

    I could not find the above data in HMC1020 datasheet.

    Please kindly help.
    Please. Can someone tell me?

  • HMC1020 SCI1-4 Configurations


    I have few questions regarding the HMC1020 RMS RF power detector that we use in
    some of our designs:

    1.       I saw that in the new datasheet of HMC1020 the number of combinations
    of the SCI1-4 logic pins was reduced (earlier the combinations went from…

  • Typo in HMC1020 Datasheet?

    On the HMC1020 logic pin description, it says, “V>0.2xVcc to disable”, not sure what that means.  Should it say V<0.2Vcc to disable?

     

  • Thermal resistance data for HMC1020

    Hi,

    My customer would like to know thermal resistance of θja, θjc and θjb for HMC1020.

    I could not find the above data in HMC1020 datasheet.

    Please kindly help.

    Thanks in advance.

  • HMC1020 - can it measure an LTE signal ?

    Hello,

    I'm trying to measure/estimate a standard LTE signal with the following characteristics:

    FDD

    BW 10MHz

    QPSK modulated

    Very low number of active data channels

    Since the HMC1020 transient responce can be configured via SCI1-4 pins  - I was…

  • What different with HMC1010 and HMC1020?

    Dear 

    Our customer want to know what different with HMC1010 and HMC1020.

    Could you tell me what different points?

    Best regards

    Lonnie Kim(ADI DFAE) 

  • Pin compatible between HMC1010, HMC1020 and HMC909

    I think that HMC1010, HMC1020 and HMC909 is a pin compatible devices.

    Is that right?

    Thanks.

  • Composite Power Detector and Envelope Detector Response Time

    I  need a power detector that measure total power of multi-carrier in 500 MHz bandwidth . Are HMC1020  and HMC1120's true RMS power mode  able to do this measurement of composite power? And also I  need to  know HMC1120's envelope detector response time…

  • RE: RF detector for 5G NR

    Hi jhshin,

    5G NR may incorporate carrier aggregation, plus more complex modulation schemes (higher QAM density). Therefore, make sure the chosen detector provides good accuracy across the full RF frequency range. HMC1020 and ADL5904 are fine for 100MHz…

  • Looking for a High Range RF RMS Detector that will Operate at Low Input Frequencies

    Question: I'm looking for an RF RMS detector with high range (greater than 40 dB) which will work at very low input frequencies. Which device would you recommend?

    Answer: There are a number of options. HMC909, HMC1010, HMC1020 and HMC1120 are dc…