• SPICE models required for HMC1013 & HMC913 sdlva chip

    Hello ,

    Hopefully you all be good. I am looking for SPICE models  for HMC1013 & HMC913 sdlva chips. 

    Thanks

  • RE: HMC1013 Eval kit

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: S parameter (300kHz-12GHz)

    HMC1013 will go as low as 500 MHz.

    There are no detectors that cover 300 KHZ to 12 GHz, that I'm aware of. You will most likely need to have two detectors one for LF and one for the higher freqs. The power detector circuits are getting beyond my scope.…

  • RE: AGC working at high frequency

    Have you looked at the SDLVA products?  They are much flatter over frequency than the traditional log amps.  Try looking at: HMC613, HMC813, HMC913 or HMC1013.

  • RE: I am looking for a power detector that could detect 5-10ns pulses of RF energy (400MHz-1.5GHz range).

    On behalf of Michiel Kouwenhoven:

    This is a challenging problem. In general there are two options:

    1) Use a Schottky detector preceded by an LNA; the LNA needs to have 25-30dB of gain and sufficiently fast response
    to gain up the Schottky detector input…

  • RE: HMC1013LP4E and HMC913 video load

    Just checked it out in the lab, HMC1013 can drive 50 ohm to full scale just fine.  Don't have the HMC913 on hand to test.

  • 3月重点推荐——民用雷达解决方案,是你的菜么?

    雷达广泛用于民用应用,从执法部门实施的汽车系统和速度监控到空中交通管制、天气和海上监控。雷达发射无线电波,然后通过其路径中的物体反射。雷达接收机处理这些反射波以确定物体的范围、角度或速度。例如,海上雷达可测量船舶方位和距离以防碰撞并进行船舶导航。在港口或海湾处,船舶交通服务雷达系统用于监控和调节繁忙水域中的船舶运动。配合飞机应答机系统一起使用的类似民用空中交通管制雷达确定相似特性,以确保飞机之间保持安全距离并协调飞行路径。

    主要挑战和系统设计考虑

    远程监控雷达,如空中交通管制、天气和海上雷达…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • 总有一款适合您——最新《RF和微波IC选型指南》PDF免费下载ing

    天线到数字以及数字到天线……ADI凭借领先的射频技术能力、系统知识与工艺技术,提供直流到90 GHz以上、涵盖整个RF信号链最丰富多样的RF IC组合。

     

    面对上千款的RF IC产品,如何选出最适合自己应用的哪一款呢?ADIRF和微波IC》最新选型指南来帮您。(附件)

     

    最新版的《RF和微波IC》选型指南主要包括RF放大器、可变增益放大器、衰减器、RF混频器、I/Q调制器和解调器、集成式收发器……


  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF