• What different with HMC1010 and HMC1020 and HMC1120?

    Could anyone clarify and give me any advice?

    Part : HMC1010, HMC1020, HMC1120

    Customer wants to change to HMC1120 due to Last Time Buy of HMC1010&HMC1020.

    I know Dynamic Range & Vdd and Vcc are different.


    1. What are the advantages, disadvantages…

  • HMC1010 performance according to the power supply voltage

    Could anyone clarify and give me any advice?

    Part : HMC1010

    My customer found that HMC1010's supply voltage should use +4.5V ~ +5.5V, the voltage area of the power supply range allowed by HMC1010's datasheet. So they ask for ADI's advice on this.…

  • HMC1010 Log slope and intercept calculation formulas

    Hi,

    My customers are considering HMC 1010.

    I got a question about calculation formula of log slope and interception.

    If we use RFBK = 4.7 KΩ, RSHUNT = 2.2 KΩ, and RSET = 24 KΩ when determining β on page 11-22, the calculation result is β = 3.33.…

  • What different with HMC1010 and HMC1020?

    Dear 

    Our customer want to know what different with HMC1010 and HMC1020.

    Could you tell me what different points?

    Best regards

    Lonnie Kim(ADI DFAE) 

  • RE: Power supply voltage of HMC1010

    Operating beyond abs max 5.6V means that it may cause irreversible damage to the device. At 5.5V, but there may be slight effects on output, but the device behavior should be consistent with the datasheet.  however, there would be less margin for failure…

  • Matching Components for HMC1010

    Question: Do you have recommendations for input matching component values for frequencies beyond those listed in the HMC1010 datasheet?

    Answer: The attached list provides recommended matching components for a variety of operating frequencies.

  • HMC1010 ENX

    Hi all,

    RF input is available, when using ENX = Hi power down mode ?

    Best regards,
    sss

  • RE: Values of HMC1010 input RLC

    The attached file has some updated information. This provides a list of recommended matching components at various frequencies. Matching recommendations for 1.8 GHz are not in this file. For 1.8 GHz, we recommend you set C2 to  2.7 pF and  L1 to  2.4 NH.

  • Pin compatible between HMC1010, HMC1020 and HMC909

    I think that HMC1010, HMC1020 and HMC909 is a pin compatible devices.

    Is that right?

    Thanks.

  • HMC1010 Frequency Range

    HMC1010 is specified to work to 3.9 GHz. Will it still work at 4.5 GHz (possibly with degraded performance)? Are there any similar devices that are specified to operate at 4.5 GHz?