• RE: HMC-MDB277

    Hello Mark

    I really appreciate for your helpful reply.

    I could understand that HMC8118 and HMC7586 can be utilized to up-convert and down-convert the input data.

    But when I reviewed the datasheet of HMC-MDB277 again, it seems that HMC-MDB277 is preferred…

  •  HMC-MDB277 performance data

    Please provide the following data for HMC-MDB277

    Input IP3, and IP2 vs LO drive and frequency

    Spurious table

    All other additional performance data. Data sheet is very thin.

    Thanks.

  • Hittite HMC-MDB277 LO frequency

    Hello~ I'd like to use a mixer for an automotive radar system.

    I have a question about the mixer whose part number is Hittite HMC-MDB277.

    When I see the datasheet of the mixer, it says LO frequency range is from 70 to 90 GHz. Is it possible to…

  • Hittite HMC-MDB277 LO input

    Hi, I have a question with LO drive of Hittite HMC-MDB277 mixer.

    My desired specs proceed as follows:

    IF frequency : 13~18 GHz

    LO frequency : 63 GHz

    RF frequency : 76~81 GHz

    Although the datasheet of the mixer says that it operates at the LO frequency…

  • Hittite HMC-MDB277 IF-RF feedthrough

    Hello,

    I'm designing up/down converter for 77 GHz automotive radar system.

    We use Hittite MDB277 mixer for

    IF frequency : 13~18 GHz

    LO frequency : 63 GHz

    RF frequency : 76~81 GHz

    Please let me know how much is the IF-RF feedthrough.

    Thank …

  • Hittite MDB277 LO-RF Feedthrough

    Hello.

    I'm designing up/down converter for 77 GHz automotive radar system.

    We use Hittite MDB277 mixer for

    IF frequency : 13~18 GHz

    LO frequency : 63 GHz

    RF frequency : 76~81 GHz

    I was worried that the LO input power of 14 dBm will affect the…

  • HMC-C032  HMC-C056 HMC-C058

    Hello,

    Do you offer or plan to offer 3D step models for the following Hittite products: the HMC-C032, HMC-C056, and the HMC-C058? Thanks.

    Best Regards.

  • HMC-abh209 / HMC-alh382 / HMC-sdd112

    Hi,

    I will use HMC-abh209 / HMC-alh382 / HMC-sdd112 in my design,

    Would you please help to provide as below?

    1. S parameter

    2. Input R + jX

    3. Output R + jX

    4. Gerber file

     

    Thanks,

  • HMC-463 and HMC-ALH244

    I’m working on a design which
    contains several Hittite HMC-463 and HMC-ALH244 amplifiers (unpackaged
    die).  Neither of these parts show a specification for second order
    intermodulation in the data sheet.  Can Hittite provide this information?
    Also, the HMC…

  • HMC-ALH364 and HMC-ALH476

    Do we have the on wafer measured S-parameter file for the following Hittite Components :

    1.HMC-ALH364

    2.HMC-ALH476

    Also I want to know whether these die are internally compensated or not for bond wire inductance.

    thanks.