• S-Parameters file HMC-C059

    Hello, I will need to S-Parameters and Performance Measurements for,

    Wideband Low Noise Amplifier Module, 1 - 12 GHz

    HMC-C059

    Best regards,

    Katherine Cortes

  • HMC-C032  HMC-C056 HMC-C058

    Hello,

    Do you offer or plan to offer 3D step models for the following Hittite products: the HMC-C032, HMC-C056, and the HMC-C058? Thanks.

    Best Regards.

  • HMC-abh209 / HMC-alh382 / HMC-sdd112

    Hi,

    I will use HMC-abh209 / HMC-alh382 / HMC-sdd112 in my design,

    Would you please help to provide as below?

    1. S parameter

    2. Input R + jX

    3. Output R + jX

    4. Gerber file

     

    Thanks,

  • HMC-463 and HMC-ALH244

    I’m working on a design which
    contains several Hittite HMC-463 and HMC-ALH244 amplifiers (unpackaged
    die).  Neither of these parts show a specification for second order
    intermodulation in the data sheet.  Can Hittite provide this information?
    Also, the HMC…

  • HMC-ALH364 and HMC-ALH476

    Do we have the on wafer measured S-parameter file for the following Hittite Components :

    1.HMC-ALH364

    2.HMC-ALH476

    Also I want to know whether these die are internally compensated or not for bond wire inductance.

    thanks.

  • HMC-SDD112 and HMC-SDD112-SX

    Hello,

    I don't understand very well the difference between HMC-SDD112 and HMC-SDD112-SX modules.

    Is it about packaging?

    Thank you

    Sandra Gomez

  • HMC-ALH444-SX and HMC-ALH444 difference

    Hello, dear all!

    please, could you clear a difference between HMC-ALH444-SX and HMC-ALH444

    https://octopart.com/hmc-alh444-sx-analog+devices-52340114

    There are no inform on the www.hittite.com.

    TIA!

  • HMC-493 and HMC-492 self oscillation

    Hello,

    I'm using the HMC-493 (divide by 4) and the HMC-492 (divide by 2) in an application such that they don't always have RF applied to their input.  I've just read the app note "Frequency Divider Operation and Compensation with no input signal…

  • Questions for the battery (HMC-T2220、HMC-T2240 )

    We would like to export the Signal genetor of HMC-T2220HMC-T2240.

    If these SG have a battery (Lithium Ion Battery: re-chargeable) or Lithium battery (Coin battery) , they might be prohibited to export.

    Then could you tell us the HMC-T2220HMC-T2240 has…

  • HMC 751 LNA Testing

    Recently I have requested a sample of HMC 751 LNA with the complete evaluation board from Analog devices that operates from 17-27 GHz with a stable gain of 25 dB. Do i need any additional components to test it? Or I can measure it directly with the VNA…