• what is the difference between HMC-579 and HMC-579SX

    Hello

    what is the difference between HMC-579 and HMC-579SX?

  • FAQ: HMC-C088 Output Load

    Q: What is the performance of HMC-C088 with a 50 ohm load?

  • Same s parameters for HMC 370 and HMC 369

    The s parameter files of HMC370 and HMC369 are same. Even though the file names are different the content is the same that of HMC369. Can you please upload the actual S parameters file of HMC370

  • RE: FAQ: Current Consumption of HMC-C584

    A: Allow for 10 mA on VSS and VDD.

  • FAQ: HMC-C088 Log Video Recovery Time and Output Rise Time

    Q: Can you distinguish the difference between Log Video Recovery Time and Log Video Output Rise Time of HMC-C088?

  • RE: HMC-ALH369 applied with photo diode

    I'm not familiar with this mode for operating an RF amplifier. I did some google searches which suggested that the 50 ohm input impedance of the RF amplifier is too low to act as a current to voltage converter (i.e. Vin(ac) = Iin(ac) * 50 ohms).  It…

  • RE: HMC-ALH435-DIE 10 Ohms on Vgg1

    Is there anyone can help with this?

    Appreciate.

  • hmc-980

    Hello,

    I would like to use the HMC-980 as an active bias controller for the HMC-1049. I see that there are generic circuits in the HMC-980 data sheet, but do you have a specific one for use with the HMC-1049? Also could you tell me if these two devices…

  • HMC-ALH364

    Do we have the on wafer measured S-parameter file for the HMC-ALH364?

    Thank you