• HMC-C029 THERMAL RESISTANCE

    Hello.

    Please teach me HMC-C029 THERMAL RESISTANCE.

    It is not mentioned in the data sheet.

    Thanks.

  • About the HMC-C029 output response time

    Hello,

    About the HMC-C029,
    How long is the response time from the input of voltage to the output of frequency?

    Regards,
    Tatsu

  • About the variation with the passage of time of HMC-C029 output frequency

    Hello,

    About the HMC-C029 output frequency,

    In the following two operations of "A" and "B", each output frequency is slightly different.

    "A":
     "5-10 GHz sweep in 2msec period" --->  2msec interval ---> "5-10 GHz…

  • HMC-C032  HMC-C056 HMC-C058

    Hello,

    Do you offer or plan to offer 3D step models for the following Hittite products: the HMC-C032, HMC-C056, and the HMC-C058? Thanks.

    Best Regards.

  • HMC-abh209 / HMC-alh382 / HMC-sdd112

    Hi,

    I will use HMC-abh209 / HMC-alh382 / HMC-sdd112 in my design,

    Would you please help to provide as below?

    1. S parameter

    2. Input R + jX

    3. Output R + jX

    4. Gerber file

     

    Thanks,

  • HMC-463 and HMC-ALH244

    I’m working on a design which
    contains several Hittite HMC-463 and HMC-ALH244 amplifiers (unpackaged
    die).  Neither of these parts show a specification for second order
    intermodulation in the data sheet.  Can Hittite provide this information?
    Also, the HMC…

  • HMC-ALH364 and HMC-ALH476

    Do we have the on wafer measured S-parameter file for the following Hittite Components :

    1.HMC-ALH364

    2.HMC-ALH476

    Also I want to know whether these die are internally compensated or not for bond wire inductance.

    thanks.

  • HMC-SDD112 and HMC-SDD112-SX

    Hello,

    I don't understand very well the difference between HMC-SDD112 and HMC-SDD112-SX modules.

    Is it about packaging?

    Thank you

    Sandra Gomez

  • HMC-ALH444-SX and HMC-ALH444 difference

    Hello, dear all!

    please, could you clear a difference between HMC-ALH444-SX and HMC-ALH444

    https://octopart.com/hmc-alh444-sx-analog+devices-52340114

    There are no inform on the www.hittite.com.

    TIA!

  • HMC-493 and HMC-492 self oscillation

    Hello,

    I'm using the HMC-493 (divide by 4) and the HMC-492 (divide by 2) in an application such that they don't always have RF applied to their input.  I've just read the app note "Frequency Divider Operation and Compensation with no input signal…