• HMC-ALH364 and HMC-ALH476

    Do we have the on wafer measured S-parameter file for the following Hittite Components :

    1.HMC-ALH364

    2.HMC-ALH476

    Also I want to know whether these die are internally compensated or not for bond wire inductance.

    thanks.

  • HMC-463 and HMC-ALH244

    I’m working on a design which
    contains several Hittite HMC-463 and HMC-ALH244 amplifiers (unpackaged
    die).  Neither of these parts show a specification for second order
    intermodulation in the data sheet.  Can Hittite provide this information?
    Also, the HMC…

  • HMC-C032  HMC-C056 HMC-C058

    Hello,

    Do you offer or plan to offer 3D step models for the following Hittite products: the HMC-C032, HMC-C056, and the HMC-C058? Thanks.

    Best Regards.

  • RE: HMC-abh209 / HMC-alh382 / HMC-sdd112

    Hi,

    How about HMC-abh209 and HMC-alh382?

    Thanks.

  • HMC

    Placeholder

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • RE: HMC-SDD112

    FormerMember
    FormerMember

    Hello,

    Our analysis on the HMC-SDD112 concluded that the typical P1dB is +24dBm.

    Former Hittite acquired the HMC-SDD112 along with the Velocium product line.

    Unfortunately, we have minimal info on the large signal/power handling performances of the…

  • HMC-ALH476 and HMC981LP3E

    We are prototyping a low noise amplifier based on the combination of an
    HMC-ALH476 and HMC981LP3E.  We are using the HMC981LP3E to set the gate voltage
    to control the drain current, using component values suggested on P18 of the
    HMC981LP3e data sheet…

  • the HMC-T2220 control software for Linux system

    I'm using Hittite HMC-T2220 Signal Generator. I want to control the HMC-T2220 with linux system,but  there is a software for controlling HMC-T2220  with windows system. Is there any suitable control software for Linux system?

  • RE: Phase Detector for Ultrasonic Circuit - 30 kHz

    Your best bet would be to use a mixer. The HMC Phase Frequency Detectors were designed specifically for synthesizer applications. Please see the HMC Phase Frequency Detector FAQ.
    FAQ: HMC Phase Frequency Detectors