• hmc-980

    Hello,

    I would like to use the HMC-980 as an active bias controller for the HMC-1049. I see that there are generic circuits in the HMC-980 data sheet, but do you have a specific one for use with the HMC-1049? Also could you tell me if these two devices…

  • RE: Need to cool for amplifier module package ?

    Both the HMC-C004 and the HMC-C016 need to be mounted to be cooled.  As stated in the outline drawing "Bottom to be held at 85 degrees C max.".

  • About HMC PLL+VCO with USB control board

    Dear Sir,

    Most of HMC EVB of PLL+VCO with USB control board whether is common for all HMC synthesizer EVB or uni for each ?

    Thanks a lot.

  • Need the weight of the HMC-C071 component

    Need the weight of the HMC-C071 component. Here is the link https://www.analog.com/en/products/hmc-c071.html to the component.

    The logistics Department for the organization of transportation requires you to specify the exact weight. Please report the exact…

  • RE: Board level alternative to HMC-C019

    Evan,

         The HMC-C019 consists of 2 HMC547 die in series.   As long as you optimized the layout for isolation there is no reason a PCB version of the HMC-C019 should not work as well.

    best regards,

    M

  • HMC7357 failing

    I have a design that uses the HMC 7357 with the HMC 980 to control the gate and drain voltage on the HMC 7357 and after a few hours to a few days of operation I am seeing the HMC7357 failing.  The HMC 7357 is operating at 7.7V and the RF drive is 0 dBm…

  • RE: HMC-MDB277

    Hello Mark

    I really appreciate for your helpful reply.

    I could understand that HMC8118 and HMC7586 can be utilized to up-convert and down-convert the input data.

    But when I reviewed the datasheet of HMC-MDB277 again, it seems that HMC-MDB277 is preferred…

  • HMC-493 and HMC-492 self oscillation

    Hello,

    I'm using the HMC-493 (divide by 4) and the HMC-492 (divide by 2) in an application such that they don't always have RF applied to their input.  I've just read the app note "Frequency Divider Operation and Compensation with no input signal…