• RE: HMC-C032  HMC-C056 HMC-C058

    Hi Bill,

    currently we DO NOT offer the 3D models for these products.

    the detailed package drawings and dimensions are included in the datasheet along with the S-parameter plots.


  • RE: HMC-abh209 / HMC-alh382 / HMC-sdd112

    Hi,

    How about HMC-abh209 and HMC-alh382?

    Thanks.

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • RE: Hittite HMC-MDB277 LO input

    Hello,

    We don't have HMC-MDB277 conversion loss data for an LO of 63 GHz.  I would expect to see conversion loss in the -16 dBm range, but may be worse.  It's probably best to test the die using your RF/LO combination to confirm the insertion loss…

  • HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.

  • Die Temperature

    How can I determine the die temperature of your device?

  • HMC392A-Die

    I wanted to Simulate the HMC392A in Microwave office. So i downloaded its S2P file from design resources and as i performed simulation its responses like return loss is better than the datasheet but its gain is decreased to max15.7 dB after simulation…