• [Urgent] Channel Temperature of HMC-APH403-DIE

    Hi

    Our customer requests the channel temperature data of HMC-APH403-DIE. Could you please let me know ?

    He compares HMC-APH403-DIE with a competitor. If he takes the data quickly, there is some chance of beating.

    Regards,

    Hiroyuki  

  • RE: Board level alternative to HMC-C019

    Evan,

         The HMC-C019 consists of 2 HMC547 die in series.   As long as you optimized the layout for isolation there is no reason a PCB version of the HMC-C019 should not work as well.

    best regards,

    M

  • RE: I am building Footprints for our Library and am looking for DXF files.

    Please create separate posts requesting die dimensions for the following products:

    HMC8410CHIPS

    HMC-ALH476

    HMC1106

    BTW, each datasheet has figures with die dimensions and bond pad locations.

  • HMC-ABH241 : Die Related- Queries

    Find both Q&A below. 

     

    1. We only show decoupling for one side of the die. The top side in the view
    below has the same supply pads. Is decoupling only on one side required and can
    it be either side?
    Yes the supplies only on south or north…

  • RE: HMC-C009 Design issue

    The HMC-C009 uses the HMC525 die.  Best advice is to ensure the Phase length  of IF! and IF2 are matched.

    best regards,

    M

  • RE: HMC-ALH364 and HMC-ALH476

    Hello ADI_Eva,

    S-parameters for the HMC-ALH476 are available on the HMC-ALH476 product page of the analog.com website. See link below:

    http://www.analog.com/media/en/simulation-models/s-parameters/HMC-ALH476.zip

    Use of a text editor to open the S-par…

  • RE: S2P file of HMCALH444

    Hi Maria,

    Below is a plot of the HMC-ALH444 noise figure vs. frequency grouped by operating temperature and DC bias. Because the HMC753LP4E is our packaged version of the HMC-ALH444 die, I've also included the noise figure plot from the HMC753LP4E data…

  • HMC-463 and HMC-ALH244

    I’m working on a design which
    contains several Hittite HMC-463 and HMC-ALH244 amplifiers (unpackaged
    die).  Neither of these parts show a specification for second order
    intermodulation in the data sheet.  Can Hittite provide this information?
    Also, the HMC…

  • I am planning to use HMC-SDD112 switch for my project . There is no way to download the s-parameter file of that component. Can you please send me the S-Parameter touchstone file for that die. I am planning to use HMC-SDD112 switch for my project . T...

    I am planning to use HMC-SDD112 switch for my project . There is no way to download the s-parameter file of that component. Can you please send me the S-Parameter touchstone file for that die. 

  • RE: HMC-APH460-DIE S-Parameter File

    Hi SMcBride,

    Thank you for the information! However, I'm looking for the S-parameters for HMC-APH460, which is a 1/2 W power amplifier in the 27-31.5 GHz band. HMC-460 is a LNA chip from DC-20 GHz. 

    Thank you for your time,


    Arthur