• HMC-ABH241 : Die Related- Queries

    Find both Q&A below. 

     

    1. We only show decoupling for one side of the die. The top side in the view
    below has the same supply pads. Is decoupling only on one side required and can
    it be either side?
    Yes the supplies only on south or north…

  • HMC-APH460-DIE S-Parameter File

    Hi,

    I am planning using the HMC-APH460-DIE in my project. I wanted to include the small signal behaviour in my system simulation. There is no available S-parameter file data available to download from the part website currently. I was wondering if there…

  • [Urgent] Channel Temperature of HMC-APH403-DIE

    Hi

    Our customer requests the channel temperature data of HMC-APH403-DIE. Could you please let me know ?

    He compares HMC-APH403-DIE with a competitor. If he takes the data quickly, there is some chance of beating.

    Regards,

    Hiroyuki  

  • RE: 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi HM,

    Unfortunately, we do not have the 2nd & 3rd harmonic data for these parts (or the IP2 data required to calculate this) at the moment.

    Thanks,

    Dan

  • I am planning to use HMC-SDD112 switch for my project . There is no way to download the s-parameter file of that component. Can you please send me the S-Parameter touchstone file for that die. I am planning to use HMC-SDD112 switch for my project . T...

    I am planning to use HMC-SDD112 switch for my project . There is no way to download the s-parameter file of that component. Can you please send me the S-Parameter touchstone file for that die. 

  • HMC-C032  HMC-C056 HMC-C058

    Hello,

    Do you offer or plan to offer 3D step models for the following Hittite products: the HMC-C032, HMC-C056, and the HMC-C058? Thanks.

    Best Regards.

  • HMC-abh209 / HMC-alh382 / HMC-sdd112

    Hi,

    I will use HMC-abh209 / HMC-alh382 / HMC-sdd112 in my design,

    Would you please help to provide as below?

    1. S parameter

    2. Input R + jX

    3. Output R + jX

    4. Gerber file

     

    Thanks,

  • AD2428WCCSZxx die revision

    Hi

    Could you kindly let us know what difference with AD2428WCCSZ and AD2428WCCSZ01?

    Our customer use AD2428WCCSZ01 first, but they want to modify to non-automotive version, but AD2428BCPZ no die revision, they confuse about it.

  • HMC-ALH364 and HMC-ALH476

    Do we have the on wafer measured S-parameter file for the following Hittite Components :

    1.HMC-ALH364

    2.HMC-ALH476

    Also I want to know whether these die are internally compensated or not for bond wire inductance.

    thanks.

  • HMC-463 and HMC-ALH244

    I’m working on a design which
    contains several Hittite HMC-463 and HMC-ALH244 amplifiers (unpackaged
    die).  Neither of these parts show a specification for second order
    intermodulation in the data sheet.  Can Hittite provide this information?
    Also, the HMC…