Hello,
I don't understand very well the difference between HMC-SDD112 and HMC-SDD112-SX modules.
Is it about packaging?
Thank you
Sandra Gomez
Q: What is the performance of HMC-C088 with a 50 ohm load?
Hello, dear all!
please, could you clear a difference between HMC-ALH444-SX and HMC-ALH444
https://octopart.com/hmc-alh444-sx-analog+devices-52340114
There are no inform on the www.hittite.com.
TIA!
I'm using the HMC-493 (divide by 4) and the HMC-492 (divide by 2) in an application such that they don't always have RF applied to their input. I've just read the app note "Frequency Divider Operation and Compensation with no input signal…
We would like to export the Signal genetor of HMC-T2220、HMC-T2240.
If these SG have a battery (Lithium Ion Battery: re-chargeable) or Lithium battery (Coin battery) , they might be prohibited to export.
Then could you tell us the HMC-T2220、HMC-T2240 has…
Hi SSifat218,
I would recommend using a Keithley DC power supply (can be purchased through Tektronix or Test Equity). The most common model we use in the lab is the 2400 series, but they are pretty pricey (~$4000). So if you want a cheaper solution they…
Hello
I am conducting differential interference analysis using HMC 702 and HMC 584, but there is a problem.The sign of the phase is changed by turning on / off the power supply.My question is· Which code of the phase is decided is PLL IC or VCO?· Is…
what is the difference between HMC-579 and HMC-579SX?
The s parameter files of HMC370 and HMC369 are same. Even though the file names are different the content is the same that of HMC369. Can you please upload the actual S parameters file of HMC370
A: Allow for 10 mA on VSS and VDD.