• HMC-ALH364 and HMC-ALH476

    Do we have the on wafer measured S-parameter file for the following Hittite Components :

    1.HMC-ALH364

    2.HMC-ALH476

    Also I want to know whether these die are internally compensated or not for bond wire inductance.

    thanks.

  • HMC-ALH364

    Do we have the on wafer measured S-parameter file for the HMC-ALH364?

    Thank you

  • HMC-ALH364 Noise Figure Measurements

    I'm looking for Noise Figure measurements of the HMC-ALH364 versus temperature (-40C, 25C and 85C). The data sheet only shows one chart with no temperature reference. Thanks! James

  • RE: HMC-ALH435-DIE 10 Ohms on Vgg1

    Hi avatar,

    1) It's in series of the path.

    2)  I would recommend a bondable resistor from AVX.

    3) The resistor in between the bypass capacitors is part of the noise filtering bypass circuit and also is there to protect the gate .

    Thanks,

    DanO

  • HMC-ABH241 : Die Related- Queries

    Find both Q&A below. 

     

    1. We only show decoupling for one side of the die. The top side in the view
    below has the same supply pads. Is decoupling only on one side required and can
    it be either side?
    Yes the supplies only on south or north…

  • HMC-APH460-DIE S-Parameter File

    Hi,

    I am planning using the HMC-APH460-DIE in my project. I wanted to include the small signal behaviour in my system simulation. There is no available S-parameter file data available to download from the part website currently. I was wondering if there…

  • [Urgent] Channel Temperature of HMC-APH403-DIE

    Hi

    Our customer requests the channel temperature data of HMC-APH403-DIE. Could you please let me know ?

    He compares HMC-APH403-DIE with a competitor. If he takes the data quickly, there is some chance of beating.

    Regards,

    Hiroyuki  

  • I am planning to use HMC-SDD112 switch for my project . There is no way to download the s-parameter file of that component. Can you please send me the S-Parameter touchstone file for that die. I am planning to use HMC-SDD112 switch for my project . T...

    I am planning to use HMC-SDD112 switch for my project . There is no way to download the s-parameter file of that component. Can you please send me the S-Parameter touchstone file for that die. 

  • HMC-C032  HMC-C056 HMC-C058

    Hello,

    Do you offer or plan to offer 3D step models for the following Hittite products: the HMC-C032, HMC-C056, and the HMC-C058? Thanks.

    Best Regards.

  • HMC-abh209 / HMC-alh382 / HMC-sdd112

    Hi,

    I will use HMC-abh209 / HMC-alh382 / HMC-sdd112 in my design,

    Would you please help to provide as below?

    1. S parameter

    2. Input R + jX

    3. Output R + jX

    4. Gerber file

     

    Thanks,