• HMC-SDD112 Mounting & Bonding Techniques

    Hi,

    The Mounting & Bonding section of HMC-SDD112 datasheet recommends to use 5mil or 10mil thick "Alumina Substrate Thin Film" to bring the RF to and from the chip. For my specific application, I want to use a 4mil thick substrtae from Rogers Corporation…

  • RE: HMC-ALH509- Vacuum and Plasma?

    Hello,

    The HMC-ALH509 can be plasma cleaned.  The air bridges are part of the GaAs HEMT fabrication process.  When you ask about vacuum, are you referring to picking the die with a vacuum tip?  The air-bridges are fairly robust but can be damaged if not…

  • HMC-ALH444

    Hello,

    Do you have any performance data or plots vs. temeperature for the HMC-ALH444 Die? I need to operate over an ambient temperature range from -20 to +70 and would like to know how the device will perform. Thanks.

    Best Regards.

  • RE: The hopping time of HMC704

    Program Reg0Ah = 1800h.  If it is left at its default value (2005h), the VCO Auto-calibration feature is enabled and will be triggered every time a frequency is programmed.  This feature is only used on HMC PLLVCO products that use the same PLL die as the…

  • RE: LOW drain current (AUH320, ALH509, HMC1144)

    Hi Jaber,

    I support the HMC1144 and can answer regarding that product, though I support neither the HMC-ALH509 nor the HMC-AUH320 and thus cannot answer for either of those products. The applications engineer(s) who support those products should soon…

  • RE: desired frequency locking problem

    I recommend you use Open mode not HMC mode (no register read back in HMC mode). 

  • RE: ADuCM355 Using AFE Clock for Digital Die

    Hi Yan-Wei,

    A couple of points to note:

    - The digital die maximum clock rate is 26MHz. This is the max clock rate the memories and digital logic were tested and qualified to. 

    - Did you follow the steps in the user guide under the section "Connecting AFE…

  • RE: HMC-SDD112 Performance

    Hi,

    The HMC-SDD112 is a part acquired from another company.  The only test data provided was the scalar s-parameters. We have not performed any large signal test (P1dB and  IP3) on this die part.

    Based on the device size, expected P1dB and expected maximum…

  • RE: HMC-ALH476 and HMC981LP3E

    Hi,

    Yes you can use HMC981LP3E to bias HMC-ALH476. In order to change the default Vgate and Vneg threshold values you need to use external resistors. R4 and R6 resistors, at the attached circuit, change the -2.5V value to -1V for this application. Circuit…

  • HMC-ALH382 RF Pad Dimensions

    Hello,

    I see in the datasheet for the HMC-ALH382 LNA that the bond pad width and gap are both 100 um (page 4), giving an effective pitch of 200 um. Would I be able to measure this device using 150 um GSG probes?

    Thanks,

    BT