• 16G low phase noise comb line

    Which is better for a low phase noise comb line at 16G, a) to double 8 to 16G with a HMC573, HMC814 or HMC561;  b) to quadruple 4G to 16G with HMC370? Assume a 4 to 8G doubler is ideal. From the data sheets, it seems the quad multiplier HMC370 has a higher…

  • Is there a +/-16g version of the ADXL362 planned?

    Hello,

    Is there a +/-16g version of the ADXL362 planned? The ADXL362 has a great feature set and the low power consumption is great. But, our application calls for measurements above 8g.

    Thank you!

  • RE: EVAL-ADXL362Z-DB Flash Programing

    Hi ,

    I have sent you an email regarding this. 

    Best regards,
    John

  • Do you have a beamformer solution at 28G Hz ( just like ADAR1000 which is beamformer at 16G Hz) ?

    Do you have a beamformer solution at 28G Hz ( just like ADAR1000 which is beamformer at 16G Hz) ? 

  • How to convert the measurement range of MPU6050 accel & gyro from +-16g / 2000 deg/sec into +- 2g / 200deg/sec?

    import smbus
    import time
    
    # Get I2C bus
    bus = smbus.SMBus(1)
    
    # MPU-6000 address, 0x68(104)
    # Select gyroscope configuration register, 0x1B(27)
    #		0x18(24)	Full scale range = 2000 dps
    bus.write_byte_data(0x68, 0x1B, 0x18)
    # MPU-6000 address…

  • RE: EVAL-ADXL362Z-DB USB Driver

    Hi ,

    Thank you for your post!

    The USB Driver is in a zip file downloadable from the FTP site. Here's the link: ftp://ftp.analog.com/pub/iMEMS_Sensor_Eval/EVAL-ADXL362Z-DB/ 


    Hope this helps!

    Best regards,
    John

  • ADXL345Z-DB

    Hi,

    I just purchased the ADXL345Z-DB development board for my school project. I'm totally new into accelerometer and stuff and I have a few questions to ask regarding ADXL345Z-DB.

    1. The accelerometer comes with user-selectable g ranges, e.g. +…

  • ADXL345Z-DB

    I purchased this board in your company web site. when i reveived it ,  it can not work correctly  after  I install the battery. only the red led 2 is lighted and no datas was writed in the sd card. what is the problem ?

    I refer to the following website…

  • EVAL-ADXL346-DB

    Dear Analog,

    I recently ordered an eval board EVAL-ADXL346-DB. I have a couple of questions:

    1) I am able to read the data out in x,y and z axis. But however this data seems like decimated data. How do I read the undecimated data out of the x,y and…

  • convert dB to signal

    I need help with Sigmastudo - ADA1466. I communicate with DSP with SPI. For setting one value I need use DC input - but value will be set in dB. How can I transfer this dB set values to signal ? I need compare two signals, but one of signal will be set…