Original Question: Simulate with an AMP03, Importing Models by alanhh
I have found that the library comes with the AMP01,02, and 04, but not the AMP03. Naturally it is the one I need. I am just now learning this particular suite and I am having trouble…
AMP03: 高速差分放大器
AMP03是一款单芯片单位增益、高速差分放大器,内置一个相匹配的薄膜电阻网络,可以在整个工作温度范围内稳定工作,无需昂贵的外部匹配元件。AMP03是差分放大器和仪表放大器的基本模拟构建模块。
AMP03: High Speed Differential Amplifier by zrk787
AMP03: High Speed Differential Amplifier
The AMP03 is a single-chip, unity-gain, high-speed differential amplifier with a matched thin-film resistor network that operates stably over the entire operating…
Hi,
I designed system thats monitoring batteries discharging.
There are a lot of batteries sampled by AMP03 (Unity gain, diff. amp) then transfered via 2 analog 32-1 MUX (ADG732) and analog MUX 2-1 (ADG1219) and finally driven through the another unity…
I am using the ADR01 to generate a 10V reference input to a DAC. I am using an AMP03 to produce the -10V reference. I was getting some glitch noise on the DAC output, so, I added a lowpass filter to the negative reference input. The reference input has…
Thank's for your attention and recommendation
I've studied many papers about VCCS. (almost all papers )
it is one of the first application notes that I had studied before
one of the worst drawback of such circuit is the mismatch between resistors…