I am using AMP01fx IC for amplifying micro volt signal from the three terminal input. The two terminals are connected to differential
input of AMP01fx and the 3rd terminal input is to be connected to Guard Drive. I need to implement Guard Drive Connection…
Hi 206_RC,
Yes, the input noise voltage AND the "0.1Hz to 10Hz" Vnoise (Vpp) are good parameters to choose for when trying to find a part that can extend the lower detection voltage range to 1uV, as in your case.
For example, you can use this…
Hi Gustavo,
I have a board that uses AMP-01 in differential configuraton. But, right now I need to use the same board (with minor modification) for amplifying an AC coupled accelerometer , ACH-01 (http://www.audiomatica.com/wp/wp-content/uploads/2012…
AD600 |
AD602 |
AD603 |
AD604 |
AD605 |
AD8264 |
AD8330 |
AD8331 |
AD8332 |
AD8334 |
AD8335 |
AD8336 |
AD8337 |
AD8338 |
ADL5246 |
ADL5330 |
ADL5331 |
LTC6412 |
HMC6187G |
HMC997G |
HMC996 |
HMC694G |
AD8368 |
AD8351 |
AD8367 |
AD75071 |
AD552… |
This webcast provides insight into the challenges engineers encounter in implementing circuits for space applications. Concerns about reliability, radiation effects and the ability to tolerate harsh environmental conditions requires special attention…