• RE: About ADuM6201 Output Voltage

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADuM6201 EMC testing failed, noise, BT communication jammed

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • 电压隔离选型

    正在做一个项目,其中有两路信号需要隔离:

    1. 0-10V可调电压信号输入,要求隔离后转换为0-10V电压信号.输入端没有任何辅助电源.输出端可以有5V,15V辅助电源.

    2.1K Hz PWM信号输出,要求隔离后转换为同等频率的PWM信号.

    看到一个客户提供的参考电路板,用的是ADUM6201实现的,想请教一下,是否可行.

    谢谢!

    王锐 18918670903 wanrense@sina.com

  • RE: digital I/O in ADuM6402

    Hi Power-man:

    The ADuM6402 inputs that are not used can be connected to GND (or to VDD).  The unused outputs should be left unconnected.

    If they only need 2 channels they could also use the ADuM6201, which has 1 forward channel and 1 reverse channel…

  • RE: Use of ADuM6211 and ADM3101E

    Hello RAnslow,

    Thank you for your answer.

    I checked your adviec for my customer but

    It is difficult for customer to add 5V supply for isolated DC-DC  only,

    so I am introducing ADuM6201 which can supply 40mA at 3.3V supply.

    Best Regards,

    Terumasa

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • 把握黄金急救时间,ADI自动体外除颤器(AED)解决方案免费下载ing!

    你知道心源性猝死(SCD)吗?

    心源性猝死是指急性症状发作后1小时内发生的以意识突然丧失为特征的由心脏原因引起的自然死亡,而且心源性猝死90%以上发生在医院外,但是这类猝死病人的黄金急救时间只有5-10分钟,超过10分钟的抢救存活率不到1%。

    当发生心源性猝死(SCD)时,唯一的救治手段是胸外按压+心脏除颤,及时除颤是迄今公认制止心脏猝死的最有效方法。

    对此,ADI推出了自动体外除颤器(AED)解决方案,可以自动诊断可能危及患者生命的心室纤维性颤动和心室性心博过速两种心律失常症状。

     PDF

    自动一词提示器件可以自主分析患者状况…

  • Value of Clearance and creepage

    Hello

    Our customer will use ADuM6402.

    Could you give me your advice what do below difference of value of clearance and creepage  mean ?

    VDE document downloaded on your web site says below.

    Clearance: Over 8.5mm

    Creepage: Over 8.5mm

    (Please refer…

  • iCoupler VDE document

    Hello

    Our customer will use ADuM6402.

    So he requests VDE document.

    We check the document of VDE 0884 on your web site .

    Its document P.1 says "valid until 2014 12 31"

    (I reffer attachment).

    Uploaded document on web site has been expired…