• RE: ADE9153A_ADUM6000

    Hi aherdia , 

    1/ the output current of ADUM6000 (for 3.3V to 3.3v isolated) is 40mA 

    2/ The consuption of ADE9153A is 12mA 

    3/ the consuption of ADUM4152 is 22.5mA 

    => the total consuption is 34.5mA

    Is correct to use ADUM6000? or choose an other component…

  • RE: ADUM5020 and ADUM5028 for RS-485 Circuit

    Hi Hakan,

    I’ve added some details below on how to use the ADM2795E with the ADuM6028 DC-DC converter.

    The small size of the ADuM6028 makes this attractive in the space constrained applications. The ADuM6028 is suitable for 3.3V transceiver supply…

  • RE: adum4151 - ade9000

    You can email me the schematics direct. If you have FAE support from Analog, please copy them also.

    The ADuM4151 does not have an integrated isolated dc/dc converter. There must be independent supplies available on the primary and secondary sides. 

    If…

  • RE: ade9153a

    Hi Belaj, 

    The quick answer is yes. The ADuM5000 can provide 60mA @ 3.3V isolated power. There are some other part and package options available depending on your application needs. So to say it with package and HV rating options, the ADuM5000/ADuM6000 can…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • 错过了新品发布?来看看2018上半年新品汇总吧

    转眼间,2018也已经踏入了炎炎的夏日,这半年的时间ADI可是一刻都没有闲着,努力地为大家带来各种各样的创“芯”科技。

    它们都来自不同的产品体系,也都将去到各行各业奉献自己的力量,接下来就让版主为大家盘点盘点咱们的“芯”品吧!

    欢迎大家留言告诉版主,这些最新的产品,你最关注哪些呢?

    业界带宽最宽的RF收发器 ADRV9009

    ADRV9009是业界首款最宽带宽并且支持现有全部蜂窝标准的RF收发器。

    该器件可在75 MHz至6 GHz的范围内调谐,支持2G/3G/4G/5G服务,提供两倍于前代器件的带宽…

  • 21合1,ADI新品年底大盘点来啦

    转眼间,桌上2018年的日历就已经撕到了后一张。

    蓦地回首,才发现,斑竹竟然还没计划今年的新品盘点,惭愧惭愧~

    不过万幸,总算是及时记起来了。

    今天斑竹就来盘点下2018年ADI发布的那些重量级新品,绝对值得你关注~

     

    业界首款混合式降压型同步控制器LTC7821

    LTC7821把开关电容器电路与一个同步降压型控制器相结合,可使 DC/DC 转换器解决方案尺寸相比传统降压解决方案锐减 50% 之多。这种改善是通过将开关频率提高 3 倍实现的 (并未牺牲效率)。或者,当工作于相同的频率时,基于…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032