Is it possible to connect the outputs of two ADuM6020-5BRIZ converters in series to achieve 5V, GND and -5V?
Is it possible to connect the outputs of two ADuM6020-5BRIZ converters in series to achieve 5V, GND and -5V?
Hey,
I am planning to use ADuM6020-5EBRIZ-RL in one of my isolated low power designs.
However the ESD ratings of the device are not mentioned in the datasheet.
I would like to know the device`s HBM as per ANSI/ESDA/JEDEC JIS-001, CDM as per JEDEC JESD22…
Hi
We know that UL and VDE are currently pending in the specification.
But we need to know when ADI can provide certification documents?
Hi !
I have a question about ADuM5020/28.
Does "-3" means output is 3.3V_typ?
And does "-5" means output is 5V_typ?
And is this typo?
Best regards
Kawa
Hi tbob,
The EVAL-2LCANRS485EBZ may be a helpful example. Its a two port (CAN & RS485) board that demonstrates layout techniques with the ADM3053 and ADM2582E. This board meets Class A. Emissions scans are available in UG-1561.
Uboti:
We submitted the ADuM6020/6026 for certification of IEC61010 3rd ed and it should happen in about 4 months.
Regards, Brian
Hi
What is different between the 5 series and the 6 series?
Although the dielectric strength seems to be different, the thickness of the insulating film and the length of the creepage seem to be almost same, so I think that both have a withstand voltage…
Hi Antoine:
Judge from the noise frequency point, ADuM6404 should be the root for noise. some application notes have been released to address the radiated emission issue with isopower technology built in, such as adding stitching capacitor or power beads…
Hi aherdia ,
1/ the output current of ADUM6000 (for 3.3V to 3.3v isolated) is 40mA
2/ The consuption of ADE9153A is 12mA
3/ the consuption of ADUM4152 is 22.5mA
=> the total consuption is 34.5mA
Is correct to use ADUM6000? or choose an other component…
Hi aherdia ,
1/ the output current of ADUM6000 (for 3.3V to 3.3v isolated) is 40mA
2/ The consuption of ADE9153A is 12mA
3/ the consuption of ADUM4152 is 22.5mA
=> the total consuption is 34.5mA
Is correct to use ADUM6000? or choose an other component…