• ADE9153A_ADUM6000

    Hi

    Can I use ADUM6000 to power ADE9153A and ADUM4152?
    The input of ADUM6000 is 3.3V and the Output is 3.3V isolated.
    In this case the output current of ADUM6000 is 40mA.
    Is 40mA used to power ADE9153A and ADUM4152?

    thanks
  • ADE9153A_ADUM6000

    Hi

    Can I use ADUM6000 to power ADE9153A and ADUM4152?
    The input of ADUM6000 is 3.3V and the Output is 3.3V isolated.
    In this case the output current of ADUM6000 is 40mA.
    Is 40mA used to power ADE9153A and ADUM4152?

    thanks
  • Comparable device to ADUM6000 but with higher efficiency

    Is there a comparable device to the ADUM6000, but with higher efficiency? The ADUM6000 has up to 31% efficiency.

  • ADE9153A_ADUM6000

    Hi aherdia , 

    1/ the output current of ADUM6000 (for 3.3V to 3.3v isolated) is 40mA 

    2/ The consuption of ADE9153A is 12mA 

    3/ the consuption of ADUM4152 is 22.5mA 

    => the total consuption is 34.5mA

    Is correct to use ADUM6000? or choose an other component…

  • ADuM6000 MTBF

    Anyone knows where I can find the MTBF of the ADuM6000? The datasheet only specifies de service life 

  • RE: ADuM6000: VDD1 3.3V VISO 3.3V: Output Load 5V Boost Converter

    Hi Brian, Thank you for the update and the assistance - the ADuM6000 Case marking is as follows:

    ADUM6000

    ARWZ

    #1322

    2627190.1

    A segment of the relevant schematic is attached below - thank you for any relevant insights.

    Best regards, Colin

  • RE: ade9153a_eval board

    I need the layout of eval board specially of ADUM6000 And ADUM4152 to know how the layout of isolater  

  • Is ADuM6000 (or ADuM5000) compliant with the USB low power suspend mode current limits?

    Is ADuM6000 (or ADuM5000)compliant with the low power “suspend mode” as defined
    for USB 2.0/3.0 (2.5mA limit in low power suspend mode).

     

    There is no support for USB suspend mode in the ADuM6000.  The ADuM5000 and
    ADuM6000 can be suspended…
  • ADuM6000 and RCin/RCsel High Level thresholds

    Logic levels on pins RCin / RCsel of ADuM6000 are not described
    in the datasheet.

    What is the minimum High voltage Threshold for these logic pins?

     

    The RCin/RCsel input is a standard digital input and has the same threshold
    levels…
  • ADuM6000 EMI @ 180 MHz

    My client is currently using the ADuM6000. Apparently after conducting RF Emission testing @ 360MHz their end product is not passing and they believe they have "pinpointed" the emissions coming from the ADuM6000. They also ordered the ADuM6000 eval board…