FAQ
Hi,
I am considering the ADuM6000.
I have a question about ΘJa.
This IC has two types of packages, 16-SOIC_IC and 16-SOIC_W.
The two packages are different, but only one ΘJa listed in Table 5 is 45 °C/W.
Are both packages ΘJa = 45 °C…
Hello,
I'm using the reference design of the evaluation board EV-ADE9153ASHIELDZ for a design of a power measuring application. As ADuM6000 stocks are low I'm thinking of using a ADuM6020 power isolater to supply a 3.3v isolated supply from a…
Anyone knows where I can find the MTBF of the ADuM6000? The datasheet only specifies de service life
Can you provide the certificates for the Safety and regulatory approvals for
ADuM6000ARWZ and ADUM4224WCRWZ?
I have an application that is using the output (Viso) of the ADuM6000 as a reference voltage for a comparator. If Vdd1 is +5.0V and Viso=Vsel, what is the expected range of output voltages? Basically, how do I stack up all of the errors listed in Table…
My client is currently using the ADuM6000. Apparently after conducting RF Emission testing @ 360MHz their end product is not passing and they believe they have "pinpointed" the emissions coming from the ADuM6000. They also ordered the ADuM6000 eval board…