• Adum5411 power supply

    In the input, just has 3.3V power supply for VDDP, VDD1 can connect to VDDP or not?

    From the datasheet of Adum5411,  said theVDD1 can connect to VDDP.

  • ADUM5411 I/O Voltage on EVAL-AD4114 is not at V(DD1)

    Hello, I have an EVAL-AD4114 I'm evaluating. It has an ADUM5411 incorporated into the board. I am not using an SDB, I'm interfacing via the arduino headers though I am not using an arduino. The board is being powered from a bench supply via J4 with 5V…

  • ADUM6411 and ADUM5411 page 7 Table 13 "Change vs. Temperature"

    I am comparing the ADUM6411 data sheet to the ADUM5411 and the only thing I see is that that on page 7 of the ADUM6411 data sheet Table 13 near the bottom it is re-organized from the ADUM5411 Table 13 and the "Change vs. Temperature" specification is…

  • ADuM5411 Output timing from VDDP input to Viso output

    Hello,

    I have a question about ADuM5411 DC/DC converter.

    Our customer ask us the timing(delay) about VDDP input to Viso output.

    Could you please offer me the waveform of VDDP and Viso ?

    Best regards,

    ysuzuki

  • RE: Isolated interface chip with power supply

    Hi lijie,

    The ADM3055E and ADM3057E are isolated signal and power CAN FD transceivers. They are in SOIC packages.

    SPI signal and power isolation could be the ADuM5411 in SSOP, ADuM5401 or ADuM6421A in SOIC, if BGA solutions are not possible for this application…

  • RE: ADuM5401 and Tri-State Input

    nirb81: What you suggested looks like it would work.  Instead of the ADuM5401, If you use the ADuM5411, which has the same function as the ADuM5401, but with only 30mA output (not 100mA output of the ADuM5401),  the ADuM5411 has a pin called VE1 which will…

  • RE: About ADUM140E0BRZ layout suggestion

    The following article shows the stack-up used for a six-layer board with multiple ADuM5411 devices, and may be a useful reference.

    https://www.analog.com/en/analog-dialogue/articles/plc-dcs-analog-input-module-breaks-barriers-in-isolation.html

    I'd also…

  • RE: 【重点推荐】通道间隔离型模拟输入解决方案

    ADuM5411详细介绍:

    ADuM5411是一款集成isoPowerRegistered隔离式DC/DC转换器的四通道数字隔离器,采用ADI的iCouplerRegistered技术,能够提供可在3.15 V和5.25 V之间调节的稳压隔离电源。

    在低功耗隔离设计中,ADuM5411无需使用单独的隔离式DC/DC转换器。利用iCoupler芯片级变压器技术,能够隔离逻辑信号和DC/DC转换器的磁性元件。因此可提供小尺寸、完全隔离的解决方案。

    ADuM5411隔离器提供四个独立的隔离通道,支持多种通道配置和数据速率。可应用于

    • RE: 完整方案分享——如何利用精密ADC AD7124-8进行热电偶采集

      可以参考ADI的系统方案APM_PLC-AI_2016

      "16-ch-ch-isolated-ai-solution-for-high-end-tcrtd-modules-apm_cn",通道间隔离TC。

      http://www.analog.com/media/cn/technical-documentation/apm-pdf/adi-plc-ai-solutions_cn.pdf

      通过AD7124+ADuM5411/5401(持续耐压VIORM = 565 V峰值…

    • TAGS LIST: Power Management

      LTM8045
      LTM8049
      LTM4651
      LTM4661
      LTM4686
      LTM4676
      LTM4686-1
      LTM4676A
      LTM4675
      LTM4677
      LTM4678
      LTM8062
      LTM8061
      LTM8052
      LTM8026
      LTM8056
      LTM8064
      LTM8054
      LTM8055
      LTM4600
      LTM4600HV
      LTM4608A
      LTM4604A
      LTM8032