• ADUM5242 Junction temperature

    Hi

    I have a question ADUM5242 Junction Temperature .

    ADUM5242 has θJa typ 80C/W.

    Do you have a θjc and Tj specs?

    Or is it the correct way to calculate using Figure 4?

    What is the calculation method at that time?

    Best Regards

    HOD

  • ADUM5242 EMI

    Hi
    I have a question ADUM5242.

    Ask about ADUM 5242ARZ-RL7.
    Connect between the output pin (pin 8: Viso) - output GND (pin 5: GNDiso)
    Although it is a capacitor, 0.1uF is connected in the recommended layout on page 13…
  • iCoupler ADuM524x CTI-value

    Hello,

    I use an iCoupler ADuM5242 in a device that is currently under test at UL.

    Regarding the safety clearances, the UL inspector does not accept the CTI value of 175V described in the document. He says it was not tested under UL and so, he cannot accept…

  • RE: ADUM5242 input ESD

    Jago91:

    The ADuM5242 input should not be left floating, this can cause it to sit at a level between the VOH and VOL levels and can give uncertain output results and draw some current at the input.  Instead, connect with a large value resistor (1M ohm)…

  • ADuM5241/ADuM5242 Power Consumption

    Are there any low power alternatives to the ADuM5241/ADuM5242? The maximum quiescent current is over 100mA!

    My requirement: 2.5kV isolation, 1.8V - 5.5V at 100uA output, lower input current draw, small package, single channel isolated feedback

    I am…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032