The datasheet for the ADUM5211 & ADuM5212 both mention "Soft Start" for the isolated supply voltage ramp up, but not provide and details characterizing the soft start. Is there any information that characterizes the turn on time for the…
The datasheet for the ADUM5211 & ADuM5212 both mention "Soft Start" for the isolated supply voltage ramp up, but not provide and details characterizing the soft start. Is there any information that characterizes the turn on time for the…
Yes, with some limits. The turns-ratio in the transformer is a little higher than 1:1 so there is a small amount of voltage gain. This is enough to allow normal power supply variance at the input while still maintain the set pint voltage at the output…
I am trying to determine much current the ADuM5211 will draw if it is operating at 1Mbps and also powering an isolated LED at 12mA. Therefore, the isolator power section is supplying about 18mA of isolated current (Idd1=2.7mA and Idd2=2.9mA max at 1Mbps…
LTM2894
|
LTM2895 |
LTM9100 |
LTM2885 |
LTM2881 |
LTM2882 |
LTM2883 |
LTM2884 |
LTM2893 |
LTM2886 |
LTM2887 |
LTM2889 |
LTM2892 |
LTC1694-1 |
LTC4300 |
LTC4310 |
LTC4302 |
LTC4305 |
LTC4304 |
LTC4303 |
LTC4306 |
LTC4307 |
LTC4307-1 |
LTC430… |
ADI 数字隔离器产品列举:
集成DC/DC转换器的双通道隔离器(1/1通道方向性):ADUM5211
http://www.analog.com/cn/products/interface-isolation/isolation/isopower/adum5211.html
ADuM5210/ADuM5211/ADuM5212 均为集成 isoPower隔离式DC/DC转换器的四通道数字隔离器,基于ADI公司的 iCoupler 技术,能够提供可在3.15 V和5.25 V之间调节的稳压隔离电源…
本参考设计中的特色产品推荐:
5.0V超低噪声、零漂移、RRIO双通道运算放大器:ADA4528-2
ADA4528-2为一款超低噪声、零漂移运算放大器,具有轨到轨输入输出摆幅。这两款器件的失调电压为2.5 μV,失调电压漂移为0.015 μV/°C,典型噪声为97 μV p-p(0…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |