FAQ
Dear Sir,
We want to use ADuM4223 in the full bridge driver application. Do you have the reference circuit for this application?
Thanks.
Best regards
NC
Hello,
The ADuM4223 normally allow for channel overlap. The ADuM4223 does not come with any deadtime control. The ADuM4223 will allow for overlap as shown in the figure.
RSchnell
Hi,
We are evaluating the ADuM4223.
Let me ask you some questions.
① Is the output a CMOS structure?
I am concerned about a short circuit in the power line of the internal structure.
(2) It is written in the data sheet that the distance between the power…
Hello Team,
I am using ADuM4223 in H-bridge for driving stepper motor ( model no.: 34HS46-5004D-E1000)
Below is schematic of stepper motor driver circuit. Here, 12V is supplied to ADuM4223 and 24V supplied to H-Bridge. Host micro controller is used for controlling…
Hello:
We found the opps for ADuM4223 replace TI's UCC21540.
But we met the pin compatible issue that pin 6 , ADI=NC and customer let it connect to GND.
One question is , if customer wouldn't re-layout and ADI can mount it without floating?
Does…
Hi,
I would like to use ADuM4223.
So, I have a question. Please help me.
Question:
I am experimenting with ADuM4223.
In this situation, the phenomenon that the IC that supplies power to the ADuM4223 broke down (supplying power to…
Hi !
I have a question about ADuM4223 VDE Characteristics.
At table 9 , it says conditions is 10kV and Characteristics is 6kV.
Why the value is different?
Does this means ADuM4223 guarantee(characterize) 6000V but with margin, ADI test 10kV?
Sorry…