• Connect with 2 jtags to 2 Processors

    I'm trying to connect with 2 jtags to 2 processors , BF547 and BF512, at the same time with no succes.

    I have no Problem to connect to each one of them separatly.

    I know that it's Posible to connect to 2 processors at the same time .

    Do you…

  • AD7865AS-2 and ad7865ASZ-2差异?

      在设计中采用AD7865 4通道ADC采集数据,由于采购问题,第一次采购的了AD7865AS-2,

    第二次采购回来的是 AD7865asz-2. 通过数据手册查看到二者没有区别,但是在使用中对于同样的

    情况采集回来的数据有大概4倍的差异,请问是正常的,还是有什么地方需要注意的?

    以下数据为对某4个通道采样后的量化数据(二者工作的状态相同,工作电压和硬件电路相同):

    AD7865AS-2             AD7865ASZ-2

    8196                        2049      

    9347                        2348

    10680                        2677

  • YCbCr(4:2:2) 8-bit output

    hi all,

    Please reslove this..

    i am using ADV76111 HDMI receiver..  and connecting it to SH7724.

    We are connecting P[15:8] pins of ADV7611 to SH7724.

    Which option is required to set YCbCr(4:2:2) 8-bit output on P[15:8]?

     

    Options to set video are…

  • ADV7611 - Force output to 4:2:2

    Hi.

    I have a board with ADV7611, and the output video must be in 4:2:2 format.

    However the input video can be 4:2:2 and 4:4:4.

    In ADV7611 Reference Manual, in page 86 said:

         For a 4:4:4 HDMI input stream to the ADV7611

              The DPP section filters…

  • LTC3862-2 is used in 12v, 33v input, output 48v 7A,When the 12v input,The output power of LTC3862-2 can reach the maximum 350w?

    LTC3862-2 is used in 12v, 33v input, output 48v 7A, When the 12v input,The output power of LTC3862-2 can reach the maximum 350w?

  • RE: LT4363IMS-2#PBF

    Hi Paolo,

    It is FU10 . FU means week 47 (Nov.) of Y2020, 10 is lot number.

  • Difference between the ADA4661-2 and ADA4666-2

    What is the major difference between the ADA4661-2 and ADA4666-2?

     

    The ADA4661-2 is designed to have a lower offset voltage (correspondingly,
    higher common mode rejection) than the ADA4666-2. The ADA4661-2 uses Analog
    Devices Inc. patented…
  • ADF4360-2, devide-by-2 option and duty

    Hi,

    I have received a question at ADF4360-2 from the customer that, "By using devide-by-2 option for 2GHz VCO output, does it result to output 1GHz of 50% duty ?"

    He said he is now having external discrete components of 1/2 dividing for VCO…

  • ADV7619 20-bit 4:2:2 pin mapping

    Hi,

    ADV7619 HW User Guide (UG-237), Pg 27 lists PIXEL PORT OUTPUT MODES.  I am interested in setting 0x8d for 20-bit SDR 4:2:2 Mode 3.  The tables in Appendix C doesn't list setting 0x8d.  Would it be similar to 0x81 which is on pg 199, Table 77, col…

  • ADA4528-2 drive AD7172-2 + 10VDC load cell

    My question is if It´s possible to connect a load cell (+10VDC supply) with zero drift amplifier ADA4528-2 (+5VDC supply) for driving diferential input of AD7172-2 AD converter.

    You can see the schematic attached.

    regards.