Hello Patrick,
The ADuM4221 secondary side supports higher supply voltage as compared to the UCC21540. Also, the CMTI rating of the ADuM4221 is higher than the UCC21540.
Regards,
Sanket
Hello Patrick,
The ADuM4221 secondary side supports higher supply voltage as compared to the UCC21540. Also, the CMTI rating of the ADuM4221 is higher than the UCC21540.
Regards,
Sanket
Hello,
I wish to use ADuM4221-1 to drive C3M0015065K SiC MOSFET. This requires to be driven at a negative voltage to ensure that it stays off when required. Can the ground B (GNDB ) of ADuM4221-1 be driven at -4V? The datasheet of ADuM4221-1 says it is compatible…
Hello,
I wish to use ADuM4221-1 to drive C3M0015065K SiC MOSFET. This requires to be driven at a negative voltage to ensure that it stays off when required. the ground B (GNDB ) of ADuM4221-1 be driven at -4V? The datasheet of ADuM4221-1 says it is compatible…
About ADUM4221/ADUM4121 magnetic isolation and VDD1 power supply
1.ADUM4221/ADUM4121 is magnetic isolation. In PCB design, it is usually close to the main transformer. Will the transformer and the internal isolation coil of ADUM4221 interfere with each…
Hi,
I am goning to distribute a common 40 MHz clock to 2 DDSs and 2 ADCs. Will AD9577 work for this purpose? If not, do you have any suggestion?
The ADC needs 5 V CLK and the DDS needs 1.8 V CLK.
My JPEG saga continue...
I am using a BF561 single core to compress a 640x480 YUV 4:2:2 image into JPEG format, employing the ADI JPEG Library tools. I am getting very poor performance compared with the reference results from the Spec Sheet. The Spec…
Hello Dave,
I am facing problems with replies to your answer, so I am oppening a new dicussion with the same title.
Please clarify your answer regarding STANAG support:
2) As I understand it, this is the same as RS-343A/EIA-343A and none of our parts…
Hello,
I installed 2x LTC6811-2 and then 1x LTC6804-2 on the same board and I don't have any voltage reference output at anytime. The functional diagram in the datasheets shows that VREF1 should be always present as it's generated from V+. VREF2 is not…
Hello,
Iam interested in implementing a MIMO 2*2 scenario where i will use 2 fpgas (1 as the transmitter and 1 as the receiver) where each one will be connected with one AD-FMCOMMS3-EBZ.
So the setup will be :
FPGA_1 + AD-FMCOMMS3-EBZ_1 =Base stati…
Can the ADV7403 output YUV 4:2:2 rather than YCbCr 4:2:2?
Thanks.
Chris