• ADuM4136 VDESAT Reference

    Hi, in our application we're using ADuM4136 with MOSFETs and I was wondering what the Vdesat 9V source is referenced to internally. The functional diagram in rev 0 of the datasheet references the internal clamp and the 9V source to VSS2. However, since…

  • ADUM4136 weird behavior

    How can you explain following behavior please:

    Status primary side:

    VI- tied to VSS1

    VDD1 +3,3V with respect to VSS1 (always guaranteed not to exceed chip limits, protected with TVS)

    VI+ valid PWM signal (+3,3V or 0V with respect to VSS1)

    /RESET low

  • ADuM4136 /FAULT and READY states

    Hi,

    I'm designing a motor driver using the ADuM4136.

    From the datasheet Table 9, I've noticed that there are some conditions under which the READY and /FAULT pins have "UNKNOWN" states.

    Can you explain this a bit more?  For instance, if…

  • Adum4136 Damage with Ready pin low

    Hi, 

    I am using the Adum4136 to drive IGBTs in DC-AC converter. The circuits have worked well but I am suffering occassionally damage of Adum4136. When it goes wrong, the fault pin keeps high and the ready pin keeps low. Some of them are damaged when…

  • Ask ADUM4136 DESAT fault under ringing condition

    Dear  Sir / Madam :

    I use ACPL-36JT in my Gate drive board design to drive IGBT model; there is DESAT fault problem on switch ringing.

    For example: 

    my High voltage is 270V;

    when switching, The switcher collector Pin can go to -10V; then ACPL-36 make…

  • RE: Is ADuM4135 suitable for high voltage SiC application? Do you have some suggestion?

    Hello,

     

    The ADuM4135 does have good performance, but we have come across cases where short bursts of RF can upset the DESAT operation of the parts causing a premature fault to register. We are working on addressing the issue. We should have an update…

  • About the Webcast

    In this webcast, we will discuss the integration process of intermittent renewable energy sources with intermittent high power loads generated by the charging of electric vehicle fleets. We will see how energy storage systems play a key role for the grid…

  • RE: Can the ground B (GNDB ) of ADuM4221-1 be driven at -4V?

    Hello,

    The ADuM4221-1 does not have DESAT protection. Our current offerings that include DESAT are the single channel ADuM4135 and ADuM4136 devices. The ADuM4137 and ADuM4138 also include DESAT, but they are much more complex parts, and include many…

  • RE: can ADuM5230 be used to drive IGBT FS450R12OE4 ?

    Hello Chenmj,

    As Brian has pointed out, the output voltage swing requirements for your system make the ADuM5230 not a suitable match. Also, let's estimate the power required to operate the gate drive. using total gate charge, we can calculate:

  • RE: ADUM7234: how to realize the current and voltage protection of MOSFET by using ADUM7234?

    Hello,

    The ADuM7234 provides a means for delivering a higher driver strength signal to the power MOSFET gates, as well as the ability to level shift the highside gate signal. This is done in an isolated fashion, allowing the primary and secondary sides…