RSchnell,
I am also facing similar issue of Fault pin going to 0 sporadically. Could you please help with this? I see small High frequency noise on fault line at the time driver switch off. Could you please provide the details
RSchnell,
I am also facing similar issue of Fault pin going to 0 sporadically. Could you please help with this? I see small High frequency noise on fault line at the time driver switch off. Could you please provide the details
I am thinking of a combination of ADuM4135 and SiC MOSFET.
Since the output current of ADuM4135 is insufficient, we are considering adding a buffer.
Do you have a reference circuit or application note for ADuM4135 + buffer?
您好!我首先使用LTspice软件对ADuM4135进行驱动和保护功能进行了仿真,这是对应的半桥电路仿真文件以及图片Draft1.asc,驱动与保护功能均正常。按照仿真中的电路在AD中绘制了原理图
,这是半桥上管驱动电路的图片。
1.测试步骤:(1)先给ADuM4135芯片供电;(2)控制DSP产生频率5kHz,占空比50%的PWM波,经过光耦隔离输出后,输入至ADuM4135芯片的VI+和VI-端口中。
2.芯片个端口测试情况:(1)VI+和VI-可检测到逻辑相反的PWM波(低电平0V,高电平5V…
Hallo Nignogs,
I am not sure if you had a reply via Email etc before. If not, sorry for delay.
DESAT Threshold is fixed inside the gate driver.
The external components and/or factors (e.g. temperature of diode, MOSFET/IGBT) can affect the voltages in your…
Hello,
1. Yes, if you want to operate to a higher current, you can change the Zener diode to a lower voltage.
2. D13 and C39 should be connected the GND2 pin on the ADuM4135. The Desat pin is internally referenced to the GND2 pin, and should not be pulled…
Hello,
R17 provides some voltage division for the 25 V supply connected with R11. This gets the Desat node in range of the acceptable voltages on the DESAT pin. R17 is not connected to the NTC pin.
RSchnell
For controlling the blanking time, we have to charge the blanking capacitor.
We are supplying the power to blanking capacitor through blanking resistor.
As per the datasheet of ADuM4135, the blanking resistor will be connected to VDD2 . Some application…
Hello,
Any Rblank that keeps the highest current below 14 mA will be fine. Your value of 1k3 is good.
RSchnell
Dear Sir/Madam,
Please let me know is edge modulation scheme or on-off keeying(OOK) modulation scheme is using in ADUM4135?
Please let me know where can i get this information?
Thanks
Srinivas