Hello Kawa,
There isn't an exact maximum frequency that the ADuM4120 can work at, but there are some limitations:
1) There is a minimum pulse width. This applies to both the on and off portions of the cycle.
2) Higher frequency operation will have…
Hi all,
is this part available in AEC-Q100 ?
Thanks.
Gerd
Hi !
I was checking ADuM4210 datasheet.
http://www.analog.com/media/en/technical-documentation/data-sheets/ADuM4120-4120-1.pdf
Also I was checking ADuM4233 datasheet.
http://www.analog.com/media/en/technical-documentation/data-sheets/ADuM3223_4223…
ADUM4120 VDD2 has been tested in 250mA and 1A.
we are evaluating this P/N, for 2A+ current ability, and Switching Frequency 200Khz. Solar PV application.
Could you tell me the power supply for VDD2 of ADUM4120 recommended value? 250mA?
we use 16pcs…
Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:
[Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in : .file_attr 1="1"; syntax error is at or near text '1'.…
Greetings!
I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…
I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…
Hello,
In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?
Best Regards,
Hello Team.
1:1 transformer applied in IF pin is expensive.
so we want to use without transformer.
is it possible that?
Can you support solutions?
thanks.
Best regards,
Josh