• RE: Power isolation for medical device

    Hi:

    I checked and the correct Halo Electronics transformer for the ADuM4070 is the TGRAD-560V8LF. The message from Halo is:

    Small quantity Stock (504 pcs.) is available at HALO USA for the TGRAD-560V8LF.  We can transfer stock to any HALO location depending…

  • RE: 能否给推荐一款电源隔离芯片,电流大于500mA的?

    目前,变压器集成在芯片内部的隔离电源的最大输出功率是500mW,如ADuM5000等。需要外接变压器的,可以实现隔离电源输出的芯片还有ADuM3070/ADuM4070,最大输出功率2.5W。如果希望使用ADuM5000这类变压器内置的芯片,可以将多片ADuM5000并联,其中一片作为master,而另外的芯片作为slave。详情请参考数据手册。

  • RE: Mosfet Drivers help needed!

    Hello Pantelis,

    The application note I sent you has a version of a bootstrap configuration. VDDA and VDDB are both powered from the same 15V supply, but the trick is the diode connected to VDDA. Whenever VOA is high and VOB is low, the GNDA will sit…

  • 简化采集系统,确保高质量,ADI 12导联ECG测量系统是这样实现的

    心电图是反映心脏兴奋的电活动过程,它对心脏基本功能及其病理研究方面,具有重要的参考价值。今天斑竹为大家带来了一款基于 ADAS1000 系列的 12 导联 ECG 测量系统,将相关解决方案分享给大家~

    基于 ADAS1000 系列的 12 导联 ECG 测量系统下载链接:https://www.analog.com/cn/design-center/landing-pages/002/reference-design/china/reference-design-adas1000ecg.html

  • 高速DAC和多片ADC电路的最佳医用隔离方案

    大家好,我想设计一个医用高速DAC激励信号源,直接通过电极作用于人体,然后用4片AD4003进行采集。整体电路需要满足IEC 60601医用仪器隔离标准。但是对于高速DAC的隔离和多片ADC的隔离,有几个疑问希望ADI的专家和版上的大牛们能帮助解决:

    1、管脚数目较多时的隔离需求。高速DAC一般具有较多的管脚数目,例如拿AD9744而言,需要14路信号,1路时钟,3路控制(MODE,SLEEP,CMODE)。一般而言,一个ADuM隔离芯片最多支持4到6路信号,那么针对高速DAC应用,至少需要3到4片ADuM隔离芯片…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032