• RE: ADuM3481 multichannel interface

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Use of CTRL1 in ADuM3481

    Hello ,

    What is the use of CTRL1 in ADuM3481.

    Regards,

    Prasanna G

  • Can i short VDD1 and VDDC1 of ADUM3481

    Hello,

    Is there any problem if i short VDD1 and VDDC1 of ADUM3481 to 3.3V(same supply).

  • What should be connected to pin VDDC1 and VDDC2 of ADUM3481

    Hello,

     

    Do i require to connect VDDC1 to VDDC2 of ADUM3481 to any supply or only to decap.

    Please review my attached schematics and give me yours feedback

     

    Regards,

    Prasanna G

  • ADuM3480 and ADuM3481

    Hello

    I would like to use this device to isolate a pc from other 12 vdc electronics on a marine vessel. Currently I have an FTDi wire ended USB cable interfacing from the pc to the marine nmea network with no isolation. My question is: since the FTDi…

  • ADuM3480/ADuM3481: how to use

    I would use ADuM3480 and ADuM3481 to interface an FPGA (Xilinx Spartan 6) with a test board and our ASIC (under test) outputs.

    The I/O lines from/to the FPGA includes, in example, two SPI channels (the first one to the test board devices, the second…

  • ADuM3481 multichannel SPI interface application issue

    Dear Sir,

    We used isolated supply for each one and ADuM3481 for isolate SPI lines, from main CPU all 2 ADC's are sharing same DIN, DOUT, Clock lines and separate CS, When U602 and U605 both on board the SPI communication is failed (As attached waveform…

  • RE: iCoupler数字隔离器&光耦合器的终极PK战!

    ADI 数字隔离器产品列举:

    集成DC/DC转换器的双通道隔离器(1/1通道方向性):ADUM5211

    http://www.analog.com/cn/products/interface-isolation/isolation/isopower/adum5211.html

    ADuM5210/ADuM5211/ADuM5212 均为集成 isoPower隔离式DC/DC转换器的四通道数字隔离器,基于ADI公司的 iCoupler 技术,能够提供可在3.15 V和5.25 V之间调节的稳压隔离电源…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • RE: ADuM7441 PCB Ground Plane

    Matt,

    We generally don't use ground/power fills on the signal layers. The inner two layers are deditcatedto GND/Power as you're doing, and we create a low impedance path for decoupling. You can see and example in the ADuM3481 eval board.

    Da…