• RE: Looking for an integrated, isolated dc-to-dc converter with the best output power.

    The ADuM3471 will provide 4 channels of digital isolation and has an integrated transformer driver and isolated PWM controller to provide up to 2W of output power at 5V in to 5V out.  There is a reference design that includes a BOM with transformer, diodes…

  • RE: Do you have 24V versions for industrial sensors?

    On behalf of David Carr:

    We have a few options for isolating 24 V power that could be paired with a discrete data or communications isolator for a 24 V system.

     

    1. Isolated µModule Converters
    2. Isolated Switching Regulators such as the ADuM3471. These…
  • 视频分享:icoupler®数字隔离器——ADUM347x

    ADI出品的iCouplerRegistered数字隔离器ADuM347x是业界首款在单封装中集成变压器驱动器和PWM(脉冲宽度调制)控制器的数字隔离器。

    ADuM3470/ADuM3471/ADuM3472/ADuM3473/ADuM3474均为四通道数字隔离器,集成PWM控制器和变压器驱动器以驱动隔离式DC/DC转换器。该DC/DC转换器基于iCouplerRegistered技术,提供2 W、3.3 V至24 V的调节隔离电源,输入电源电压为5.0 V或3.3 V。这样在2 W隔离设计中,无需使用单独的隔离式DC/DC转换器。

  • RE: 4~20mA方案 AD5421

    不太明白您的接法,是想用外部+24V供电DAC?

    AD5421内置降压模块的,可以参考下CN0267。只需Iout/Vout输出,建议用AD5748

    http://www.analog.com/cn/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/CN0267.html

    SPI侧跟DAC是隔离的吧?那建议您参考下我们的CN0321

    http://www.analog.com/media…

  • ADum347X overshoot

    Hi,

    I'm using 3 off ADuM3471s and 1 off ADuM3473 on a single PCB.  When power is applied I see an output voltage overshoot of approx 50%, so that the 3 off 5V/5V converters reach 7.5V, and the 5V/12.5V converter 18V .

    The peak is reached about 1…

  • 视频分享:icoupler 数字隔离器——ADUM347x

    视频分享:icoupler®数字隔离器——ADUM347x by ADIForum

    ADI出品的iCouplerRegistered数字隔离器ADuM347x是业界首款在单封装中集成变压器驱动器和PWM(脉冲宽度调制)控制器的数字隔离器。

    ADuM3470/ADuM3471/ADuM3472/ADuM3473/ADuM3474均为四通道数字隔离器,集成PWM控制器和变压器驱动器以驱动隔离式DC/DC转换器。该DC/DC转换器基于iCouplerRegistered技术,提供2 W、3.3 V至24 V的调节隔离电源…

  • 亮相幕展的 8 款领先解决方案,为你诠释如何加速迈向工业 4.0

    大家都知道慕尼黑上海电子展吧?ADI作为受邀展商之一,在展会上展示了在工业方面的领先解决方案,旨在助力加速迈向工业4.0哦~

    今天,斑竹就给大家介绍下此次幕展上ADI秀出的八款明星级解决方案哦~

    1. ADI 无线状态监控解决方案

    工业4.0当前的实现形式是基于条件的监控。ADI的MEMS振动传感器与精密转换器、线性、隔离和电源技术相结合,已经用于提供高质量机器健康数据,以便最大限度地延长机器正常运行时间并提高效率。

    可部署不平衡轴加载电机和平衡轴加载电机方案从ADXL1002采集振动数据,使用ADuCM4050处理原始数据…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • 用于多路抽头输出隔离电源的简易解决方案

    作为系统硬件设计工程师的您,是否还在为选择高性价比的多路电源输出的隔离方案而苦恼呢?比如说+15V, -15V, +5V的三路隔离电源输出, 在大多数情况下,凡是用到运放(AMP),模拟开关(MUX)和模拟量驱动输出(+/-10V,+/-20mA)的时候都会需要用到它,而系统隔离往往又是增强工业产品可靠性的重要保证。如果您目前还不具备专业的电源设计经验,特别是变压器参数方面的设计,您的首选可能会是购买隔离电源模块,优点是体积小,使用方便,但是市面上能够直接支持+/-15V,+5V多路输出的隔离电源模块的种类非常少…

  • Generating 3 Voltages with ADuM347x

    Is it possible to draw 5(10)mA on VDD2 (5V)?
    What is the max. current that can be drawn on VDD2?

     

    Per the datasheet, table 4, the max current on VDD2 is 50mA, but this total
    includes the internal current to supply the side 2 channels…