• ADuM3400 & ADuM140E1 Internal ESD enhancements

    Hi

    I am considering latchup on the ADuM3400 and ADuM140E1.
    I have two questions.

    ① According to AN-793, ADuM3400 has improved design of ESD enhancements.
    Is this design improvement applied to the ADuM140E1?

    ② Does the ADuM3400 and ADuM140E1 have the transient…

  • ADuM1400 & ADuM3400 ESD HARDENED

    Hi

    A customer asks me about the ADuM3400.

    The ADuM3400 is said to have better ESD immunity in the system than the ADuM1400.
    (By ADuM3400 Datasheet & AN-793)

    In the link below, there is no problem with 8kV for contact discharge and 15kV for air discharge…

  • (ADuM3400)What is the difference between ADuM3400 & ADuM3400-EP?

  • RE: Isolating JTAG with ADUM3400

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADuM3400 NC pin

    Hello ,

    I have a quick question on the ADuM3400 NC pin (pin 7).

    Q:  Is the ADuM3400 NC pin (pin 7) internally connected?

          If not, could connecting it to VCC1 cause any problem?

    Thanks.

    Best Regards,

    Lux

  • ADUM3400 - Output Enable VE2 Maximum Value

    Hallo,
    I have a question about the Absolute Maximum Rating (ADMU3400 Datasheet rev.E, pag.14): does the maximum value of VE2 be lower than VDD1+0.5V as indicate in the datasheet? Or is it a mistake, e.g. VDD2+0.5V?
    Thank you for your support.

  • FIT rate for ADuM3400

    Dear Sir/Madam,

    Which is the master(input)side FIT rate on your following web site for ADuM3400?

    I found 2 FIT rates there.

    http://www.analog.com/Reliability_Data/CDA/RD_WaferFab_Results.asp

    Our customer is studying your FIT rate due to take…

  • ADuM3400和ADuM1400的ESD耐压等级分别为多少!

    如题所示,ADuM3400相对于ADuM1400进行了ESD增强,但增强后的ESD能力能够达到什么等级,相关手册中并未给出。

  • ADUM3400和ADUM1400

    两种型号磁隔有什么区别?可以相互替换吗?

  • Fan out for ADUM3400

    Hello,

    I'm using ADUM3400 as a digital isolator for the project. I want to connect 12 DAC ICs (Microchip make) to the out channel of ADUM3400.

    But I'm not sure if this is the correct way to drive these many ICs logic gate from a single logic gate…