Hi,
I have a question about ADuM160N / 161N.
The D / S has the following explanation.
"Double Protection, 3000 V rms Isolation Voltage"
Hi,
I have a question about ADuM160N / 161N.
The D / S has the following explanation.
"Double Protection, 3000 V rms Isolation Voltage"
Hi,
I am using two ADuM160N digital isolators in my PCB design. I am providing digital output signals from microcontroller to the input pins of both the isolator and this digital output signal is common to input pins of both the isolator.
My design requires…
I don't see any explicit affirmation in the datasheet that VDD1 and VDD2 are completely independent.
I tried VDD1=3.3V, VDD2=5V on the bench and everything seemed fine. But in our application both VDD1 and VDD2 are not set in stone and might change…
Hi,
Yes, ADN4650 can pass the high-speed signals. In order to pass the low power signals, a standard isolator like ADuM160N is needed, though the signal levels are 1.2V so use a level shifter like ADG3308. On the output side of the isolators, it's more…
LTM2894
|
LTM2895 |
LTM9100 |
LTM2885 |
LTM2881 |
LTM2882 |
LTM2883 |
LTM2884 |
LTM2893 |
LTM2886 |
LTM2887 |
LTM2889 |
LTM2892 |
LTC1694-1 |
LTC4300 |
LTC4310 |
LTC4302 |
LTC4305 |
LTC4304 |
LTC4303 |
LTC4306 |
LTC4307 |
LTC4307-1 |
LTC430… |