• Сurrent consumption ADUM141E and ADUM1401

    Hi,

    The client is using ADUM1401, but he wants to change to a newer ADUM141E. But he says that AdUM141E has a higher current consumption than ADUM1401, and a lot of heat dissipation. 
    Data rate 2 MHz, continuous data transfer mode. Source of 8 channels…

  • Technologies node between ADUM141E and ADuM141ES

    Hi There,

    I notice both ADUM141E and ADuM141ES are produce based 0,18um CMOS process technologies.

    Is both device manufacture based on the same die but package different.

    For ADuM141ES has gone thru radiation test while  ADUM141E is package for automotive 

  • Why use an isolator like ADuM141 in my DAQ signal chain?

    Why use an isolator like ADuM141 in my DAQ signal chain?

  • ADuM141ES IBIS

    Where can I find IBIS model for ADuM141ES? Or it is the same as for ADuM141E?

  • RE: ADuM141E ESD performance

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADuM141E working at 9MHz

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • (ADuM141/142)Can you tell me the ESD diode circuit for each device?

    Hi !

    I asked about other device at past but now, our customer will use ADuM141/2.

    https://ez.analog.com/interface-isolation/f/q-a/86884/adum1280-adum1281-adum3190-can-you-tell-me-the-esd-diode-circuit-for-each-device?

    Can you tell me the ESD diode circuit…

  • RE: ADUM141 Timing with 1.8V/5V supply and reduced temperature range

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADuM141  not used pin

    Hello

    3ch only of ADuM141 4ch is used.

    How should we connect not used pin of the other 1 ch ?

    Input pin : Pull down  through about 10 K ohm ?

    Output pin: Open ?

    Please let me know your advice.

    Regards,

    Terumasa

  • ADuM141E  Output Enable Propagation Delay

    Hello

    Our customer will use ADuM141E.

    Then,  he asks output enable propagation delay of ADuM141E  if the delay is within  ~ 50ns .

    ADuM141E datasheet does not say this parameter but other product, for example  ADuM3440, describes  its parameter in the datasheet…