• ADUM140D

    Hi,

    Input voltage is 1.8V, Output voltage is 3.3V . Can I use  ADUM140D as level shifter ?

  • Voltage translation using ADuM140D

    Reading the data sheet of the ADuM140D it seems possible to use the device as voltage translator between two different circuit sections (i.e. Vdd1 @ 5 V and Vdd2 @ 3.3 V), but all the specs are referred to the condition Vdd1=Vdd2, at 3 different voltages…

  • ADUM140D: input disable delay

    Hello

    What is the typical & maximum delay for the input disable of the ADUM140D Digital Isolator?

    Thanks

    Haje

  • RE: ADuM140D Do issue

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • How to use the ADuM140D

    Hi all,

    I am trying to use the add isolation into a circuit I am designing.

    For the digital signals, I have used the ISO7640FMDW and for the analog signal, I have the DA102JC audio transformer.

    I now want to change the transformer with the ADuM140D…

  • RE: AD7175-2 communication delay issue with isolator ADuM140D

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADI New OOK Digital Isolator Cross Reference Table

    Hi Jacky,

    We don't have such a comparison table now, but in the datasheet of ADuM140D/ADuM140E you will find that "ADuM140E1 pin compatible with ADuM1400" rather than ADuM1410.

    Regards,

    Neil

  • (ADuM14x)Can ADuM14x QSOP guarantee 3kVrms-1min ?

    Hi 

    I have two questions about ADuM14x insulation.

    Q1)

    ADuM14x had already passed 3kVrms insulation standard.

    Can I say to my customer that ADuM14x(QSOP) can guarantee 3kVrms-1min ?

     

    Q2)

    And at the datasheet page 14, this is written.

    In accordance…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • RE: AD7606-4 Running Hot and Stuck in BUSY

    Harry

    My digital inputs are driven by ADuM140D isolators, so they are always connected, and fail safe to logic High if not driven by firmware. This means that ALL my digital inputs were held High for an extended period (days!); I'm not sure if this would…