• AD7124 and ADUCM363 Transicion Time

    Hi,

    I would like to use Ad7124 or ADUCM363 for ADC.

    So, I have a question.

    AD7124 or ADUCM363 has a built-in MUX, but how much is the Transicion time for that channel?
    I looked at the data sheet, but I was not able to find a particular value, so I was…

  • Are they  same verify command for ADuCM362 and ADuCM363

    According  http://www.analog.com/media/en/technical-documentation/application-notes/AN-1160.pdf

    ADuCM362 and ADuCM363 Verify command should be same. But now I encounter verify step3 command failed on  page 1 to page 4 (start page address 0, 2048, 4096,6144…

  • ADC channel change (AIN)

    Why are the AIN1,2 and AIN3,4 values ​​different when nothing is physically connected to the Aducm363 ADC channel?
    I checked in the process of receiving 16 data for each AIN channel.

    I have attached the photo below.
    If it's wrong, I'd appreciate it if…
  • AD5686R Output voltages are not as expected

    Using EVALAD5686R with ADuCM363 micro controller in SPI mode, with 2.5 reference voltage.
    DAC converted voltages are not as expected in few data point. Could you please suggest what might be going wrong?
    Below are the data

  • RE: Migrating from ADuCM360/1 to 362/3

    Hi,

    The User Guide for the ADuCM362/3 with the registers for the ADCs can be accessed here: ADuCM362/ADuCM363 Hardware Reference Manual (Rev. A) (analog.com)

    Kind regards,

    Raquel

  • RE: ADIChip.ini for ADuCM362/3 is needed

    Hi,

    If you go to the folder where CM3WSD is installed you will see an ADIChip.ini file.

    Can you try to copy and paste the [ADuCM360] and [ADuCM361] sections and rename these new sections as [ADuCM362] and [ADuCM363] so it looks like the screenshot below…

  • Mux control through Adcum363

    Hello.

    It is connected to Aducm363 I/O port for 16:1 Mux Selection.

    There are 16 temperature sensors connected to the MUX.

    Note. ADG1607 16:1 Mux product was used.

    I want to obtain data from the first temperature sensor connected to the MUX through…

  • RE: ADUCM360 IAR CONFIGURATION SETTINGS HELPPPPPPPPP

    Hi,

    I had run the Blink code at  ftp://ftp.analog.com/pub/MicroConverter/ADuCM36x_2015/ADuCM362%20Customer%20Examples/examples/Blink/

    on EVAL-ADuCM362-ADuCM363 board.

  • RE: ADuCM362 ENOB

    Hi,

     Refer to table 4 and table 5 of ADuCM362/ADuCM363(Rev 0) datasheet. 

    (ADuCM362 Datasheet and Product Info | Analog Devices)

    Regards,

    Akila

  • RE: ADuC847 noise

    Hi Henrique, 

    Apologies for the delay in getting back to you.  I see that you've received correspondence on a separate thread below.  

    Moving from ADuC847 to ADuCM363 - Q&A - Precision Microcontrollers - EngineerZone (analog.com)

    While the ADuC847…