Hi,
For ADuCM362 also,
The difference between AVDD and IOVDD must be ≤0.3 V.
Regards,
Akila
Refer to table 4 and table 5 of ADuCM362/ADuCM363(Rev 0) datasheet.
(ADuCM362 Datasheet and Product Info | Analog Devices)
Hi ADI guys,
We use Keil4 as programming tool ,but there only aducm360 and aducm361 in keil4, we didn't find aducm362 in keil4 resouce, so how to program Aducm362 in Keil4?
Thanks a lot
We use Keil4 as programming tool ,but there only aducm360 and aducm361 in keil4, we didn't find aducm362 in keil4 resouce,
so how to program Aducm362 in Keil4?
Is there a way to program hex file into ADuCM362 without IAR or Keil? I don’t find any on its homepage. The Crosscore Serial Flash Programmer 1.2.0 doesn’t support ADuCM362. #ADuCM362
Can you provide me with the adichip.ini file? I am working with the ADuCM362.
How to wake up ADuCM362 form Hibernate Mode with wake-up timer working in period mode?
Currently using ADUCM362. UART working using RX receive buffer interrupt. I would now like to use Modem Status Interrupt (change to CTS line) to generate the UART interrupt. I turn off all other interrupts to the uart and enable the modem status interrupt…
Can anyone explain/provide sample code on how to "talk" to a microcontroller (such as ADuCM362) using a terminal program such as PuTTY or Termite on a Windows machine. For example, how do I output the results of digitizing a signal to a terminal…
1.What's the impact of ADUCM362's singal end /Differential input for ADC measure?
2.What's the ppm parameter of interner Internal watch crystal?
3.Is there any setting guide file for sinc filter?
4. In our eval sample code file (ADUCM362…